Logo
25.09.00-pvw1
MCUXpresso SDK Project v: latest
Document Release Versions
25.09.00-pvw1
25.06.00
25.06.00-pvw2
25.06.00-pvw1
25.03.00
latest

Introduction

  • MCUXPresso SDK

Getting Started

  • Github Repository
  • Zip Package

User Guide

  • Drivers
  • Examples
  • Middleware
  • RTOS
  • Boards

Development

  • Build And Configuration System
  • Developing with MCUXpresso SDK

Releases

  • Release Notes
mcuxsdk
  • Docs »
  • Touchlink Commissioning events
  • Open on Repo Report an issue

Touchlink Commissioning events

Touchlink Commissioning cluster events that result from receiving Touchlink requests and responses must be handled at the application level (while events that result from Commissioning Utility requests and responses are handled by the ZCL).

When a Touchlink request or response command (e.g. a Scan Request) is received by a node, a stack event is generated which is wrapped in a tsZCL_CallBackEvent structure. In this structure:

  • eEventType field is set to E_ZCL_CBET_CLUSTER_CUSTOM

  • sClusterCustomMessage field’s tsZCL_ClusterCustomMessage structure is filled in by:

    • setting u16ClusterId to ZLL_CLUSTER_ID_COMMISSIONING

    • pointing pvCustomData to the payload data of the received command

      • The above structure is described in Section 6.1.15.

The payload data contains a command ID, which uses one of the enumerations listed in Section 44.6.1. The event is passed to the ZCL event handler which checks that the command ID is valid for the target endpoint. If it is valid, the user-defined callback function is invoked that was specified through the function eZLL_RegisterCommissionEndPoint(). The callback function can access the payload through the tsCLD_ZllCommissionCustomDataStructure structure, which is created when the above function is called.

Thus, the above user-defined callback function must be designed to handle the relevant Touchlink events:

  • For a request, the callback function may need to populate a structure with the required data and send a response using the appropriate response function, e.g. by calling eCLD_ZllCommissionCommandScanRspCommandSend() to respond to a Scan Request.

  • For a response, the callback function may just need to extract the returned data from the event.

Alternatively, the callback function may simply notify the main application of the received command and provide the payload, so that the application can process the command.

Touchlink command events

The events that can be generated for Touchlink are listed and described below (the enumerations are defined in the structure teCLD_ZllCommission_Command, shown in Section 44.9.1).

Event

Description

E_CLD_COMMISSION_CMD_SCAN_REQ

A Scan Request has been received (by server)

E_CLD_COMMISSION_CMD_SCAN_RSP

A Scan Response has been received (by client)

E_CLD_COMMISSION_CMD_DEVICE_INFO_REQ

A Device Information Request has been received (by server)

E_CLD_COMMISSION_CMD_DEVICE_INFO_RSP

A Device Information Response has been received (by client)

E_CLD_COMMISSION_CMD_IDENTIFY_REQ

An Identify Request has been received (by server)

E_CLD_COMMISSION_CMD_FACTORY_RESET_REQ

A Reset To Factory New Request has been received (by server)

E_CLD_COMMISSION_CMD_NETWORK_START_REQ

A Network Start Request has been received (by server)

E_CLD_COMMISSION_CMD_NETWORK_START_RSP

A Network Start Response has been received (by cli-ent)

E_CLD_COMMISSION_CMD_NETWORK_JOIN_

ROUTER_REQ

|A Network Join Router Request has been received (by server)| |E_CLD_COMMISSION_CMD_NETWORK_JOIN_

ROUTER_RSP

|A Network Join Router Response has been received (by client)| |E_CLD_COMMISSION_CMD_NETWORK_JOIN_

END_DEVICE_REQ

|A Network Join End Device Request has been received (by server)| |E_CLD_COMMISSION_CMD_NETWORK_JOIN_

END_DEVICE_RSP

|A Network Join End Device Response has been received (by client)| |E_CLD_COMMISSION_CMD_NETWORK_UPDATE_REQ|A Network Update Request has been received (by server)|

Parent topic:Touchlink Commissioning events

Commissioning Utility Command Events

The events that can be generated for the Commissioning Utility are listed and described below (the enumerations are defined in the structure teCLD_ZllUtility_Command, shown in Section 44.9.2).

Event

Description

E_CLD_UTILITY_CMD_ENDPOINT_INFO

An Endpoint Information command has been received (by client)

E_CLD_UTILITY_CMD_GET_GROUP_ID_REQ_RSP

A Get Group Identifiers Request has been received (by server) or a Get Group Identifiers Response has been received (by client)

E_CLD_UTILITY_CMD_GET_ENDPOINT_LIST_REQ_RSP

A Get Endpoint List Request has been received (by server) or a Get Endpoint List Response has been received (by client)

Parent topic:Touchlink Commissioning events

Parent topic:Touchlink Commissioning Cluster


Copyright 2025, NXP. Last generated on Jul 17, 2025 16:25+0200; branch release/25.09.00-pvw1, revision b64f8fe5049b66fd3bf22464fb88e71ddf73d6ec.