fxls8974cf_interrupt
Overview
The FXLS8974CF POLL example application demonstrates configuring FXLS8974CF sensor in interrupt Mode using I2C interface.The example demonstrates configuration sensor registers reguired to put the sensor in Interrupt mode, wait for data ready event and read out samples. The dataready event is routed to INT pin when samples are available sensor reads samples.