lpacmp_interrupt
Overview
The lpacmp_interrupt example shows how to use interrupt with lpacmp driver.
The lpacmp_interrupt example illustrates how to use interrupts in the lpacmp driver. In this example, the user should specify a channel that provides the voltage signal which can be controlled by the user as a sample input to lpacmp. When running the project, typing any key in the debug console will start the comparison. The interrupt occurs when the value of we check is higher than the reference value.