Overview
The ROM API project is a simple demonstration program of the SDK ROM API driver.
The ROM API supports the Serial NOR FLASH programming via the FlexSPI NOR API.
Hardware requirements
Micro USB cable
RD-RW612-BGA board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
Example will print version, perform various FlexSPI flash operation (read, program, erase). When the example runs successfully, the following message is displayed in the terminal.
ROM API FlexSPI Driver version [0x 10802]
FlexSpi flash Information:
FlexSpi flash size: xx KB, Hex: (xx)
FlexSpi flash sector size: xx KB, Hex: (xx)
FlexSpi flash page size: xx B, Hex: (xx)
Finished executing ROM API FlexSPI Driver examples