Hardware requirements

  • USB Type-C cable

  • MCIMX93AUTO-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

No special settings are required.

Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo

  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J26 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board to begin running the example.

Note: This example has to be run on CORTEX-M boot mode(SW1301:[10x1]).

Running the demo

When the demo runs successfully, will get the similar messages on the terminal.

TRDC example start
Set the MRC selected memory region not accessible
Violent access at address:  0x     100
The MRC selected region is accessible now
Set the MBC selected memory block not accessible
Violent access at address: 0x47400000
The MBC selected block is accessible now
TRDC example Success