Router
The table below lists the LED states for Router device type.
LED1 |
LED2 |
NOTES |
|---|---|---|
OFF |
OFF |
The device is not on the network |
OFF/ON (Current ON/OFF cluster status) or Blinking ON/OFF (Identifying) |
Blinking ON/OFF every 250 ms |
Network Steering/permit join is active |
OFF/ON (Current ON/OFF cluster status) or Blinking ON/OFF (Identifying) |
Blinking ON/OFF every 2 seconds |
OTA aborted or failed |
OFF/ON (Current ON/OFF cluster status) or Blinking ON/OFF (Identifying) |
Blinking ON/OFF every 500 ms |
OTA in progress |
Parent topic:LED indication table