tsCLD_ZllCommission_IdentifyReqCommandPayload
This structure is used to hold the payload data for a Touchlink Identify Request command.
typedef struct
{
uint32 u32TransactionId;
uint16 u16Duration;
} tsCLD_ZllCommission_IdentifyReqCommandPayload;
where:
u32TransactionIdis the 32-bit Inter-PAN Transaction Identifier of the request. This is a random number generated and inserted automatically.u16Durationspecifies the length of time (in seconds) that the target node is to remain in identify mode. The possible values are:0x0000: Exit identify mode immediately
0x0001–0xFFFE: Number of seconds to remain in identify mode
0xFFFF: Remain in identify mode for the default time for the target node
If the target node is unable to provide accurate timings, it will attempt to remain in identify mode for as close to the requested time as possible
Parent topic:Structures