tsSE_PricePublishPriceCmdPayload
This structure is used to hold price information to be added to a price list of a Price cluster:
typedef struct {
uint8 u8UnitOfMeasure;
uint8 u8PriceTrailingDigitAndPriceTier;
uint8 u8NumberOfPriceTiersAndRegisterTiers;
uint8 u8PriceRatio;
uint8 u8GenerationPriceRatio;
uint8 u8AlternateCostUnit;
uint8 u8AlternateCostTrailingDigit;
uint8 u8NumberOfBlockThresholds;
uint8 u8PriceControl;
uint16 u16Currency;
uint16 u16DurationInMinutes;
uint32 u32ProviderId;
uint32 u32IssuerEventId;
uint32 u32StartTime;
uint32 u32Price;
uint32 u32GenerationPrice;
uint32 u32AlternateCostDelivered;
tsZCL_OctetString sRateLabel;
} tsSE_PricePublishPriceCmdPayload;
where:
u8UnitOfMeasureindicates the resource (e.g. electricity) and unit of measure (e.g. kWh) for the pricing (see Section 42.10.3)u8PriceTrailingDigitAndPriceTieris an 8-bit bitmap indicating the price tier and the number of digits after the decimal point in the price:The 4 most significant bits give the number of digits to the right of the decimal point in the price
The 4 least significant bits give the price tier in the range 1 to 6
u8NumberOfPriceTiersAndRegisterTiersis an 8-bit bitmap indicating the number of price tiers available and the particular tier that the price information in the structure relates to:The 4 most significant bits give the number of available price tiers in the range 0 to 6
The 4 least significant bits give the price tier used in the range 1 to 6
(this value must be less than or equal to the value in the 4 leading bits)
u8PriceRatio(optional) is the ratio of the price quoted inu32Priceto the ‘normal’ price offered by the utility company. The actual price ratio should be multiplied by 10 for encoding this field, so that a field value of 0x01 represents 0.1 and 0xFE represents 25.4, while 0xFF indicates that the field is not usedu8GenerationPriceRatio(optional) is the ratio of the price quoted inu32GenerationPriceto the ‘normal’ price offered by the utility company. The actual price ratio should be multiplied by 10 for encoding this field, so that a field value of 0x01 represents 0.1 and 0xFE represents 25.4, while 0xFF is reserved to indicate that the field is not usedu8AlternateCostUnit(optional) is an 8-bit bitmap indicating the unit for the alternative cost inu32AlternateCostDelivered. Currently, the only supported unit is kilograms of CO2, indicated by the value 0x01u8AlternateCostTrailingDigit(optional) is an 8-bit bitmap in which the 4 most significant bits indicate the number of digits after the decimal point inu32AlternateCostDelivered(the 4 least significant bits are reserved)u8NumberOfBlockThresholdsis reserved for future use (for Block mode)u8PriceControlis reserved for future use (for Block mode)u16Currencyindicates the currency (e.g. Euro) used for the price - this field should be set to the appropriate value defined by ISO 4217u16DurationInMinutesindicates the duration, in minutes, for which the price will be valid (0xFFFF indicates that price will remain valid until changed)u32ProviderIdis an identifier for the utility companyu``32IssuerEventIdis a unique identifier for the price information - the higher its value, the more recently the price information was issued (a UTC time-stamp could be used in this field)u``32StartTimeindicates the start-time (UTC) for the price, in seconds. The special value 0x00000000 denotes a start-time of ‘now’u``32Priceis the resource price per unit indicated inu8UnitOfMeasure, expressed in the currency indicated inu16Currency, with the position of the decimal point as indicated inu8PriceTrailingDigitAndPriceTie``ru``32GenerationPrice(optional) is the resource price per unit indicated inu8UnitOfMeasure, expressed in the currency indicated inu16Currencyand with the position of the decimal point as indicated inu8PriceTrailingDigitAndPriceTier, for a resource that is generated on the customer premises and supplied to the utility company (e.g. solar-sourced electric power supplied to the national grid). A value of 0xFFFFFFFF indicates that this field is not usedu32AlternateCostDelivered(optional) indicates an alternative cost (per resource consumption unit) which is measured by a means other than monetary - for example, the amount of CO2 emitted per unit of gas consumed This alternative cost is interpreted as specified byu8AlternateCostUnitandu8AlternateCostTrailingDigitsRateLabelis a string of up to 12 characters containing a label for the price information in the structure
Parent topic:Structures