tsCLD_CommissioningCallBackMessage
For a Commissioning event, the eEventType field of the tsZCL_CallBackEvent structure is set to E_ZCL_CBET_CLUSTER_CUSTOM. This event structure also contains an element sClusterCustomMessage, which is itself a structure containing a field pvCustomData. This field is a pointer to the following tsCLD_CommissioningCallBackMessage structure:
typedef struct
{
uint8 u8CommandId;
union
{
tsCLD_Commissioning_RestartDevicePayload
*psRestartDevicePayload;
tsCLD_Commissioning_ModifyStartupParametersPayload
*psModifyStartupParamsPayload;
} uReqMessage;
union
{
tsCLD_Commissioning_ResponsePayload
*psCommissioningResponsePayload;
} uRespMessage;
} tsCLD_CommissioningCallBackMessage;
where:
u8CommandIdindicates the type of Commissioning command that has been received by a cluster server or client (the same enumerations are used for requests on the server and responses on the client), one of:E_CLD_COMMISSIONING_CMD_RESTART_DEVICE
E_CLD_COMMISSIONING_CMD_SAVE_STARTUP_PARAMS
E_CLD_COMMISSIONING_CMD_RESTORE_STARTUP_PARAMS
E_CLD_COMMISSIONING_CMD_RESET_STARTUP_PARAMS
uReqMessageis a union containing the payload of a request command in the following form:psRestartDevicePayloadis a pointer to a structure containing the Restart Device command payload - see Section 43.9.2psModifyStartupParamsPayloadis a pointer to a structure containing the (common) payload for the Save Start-up Parameters, Restore Start-up Parameters and Reset Start-up Parameters commands - see Section43.9.3
uRespMessageis a union containing the payload of a response command in the following form:psCommissioningResponsePayloadis a pointer to a structure containing the (common) payload for the Save Start-up Parameters, Restore Start-up Parameters and Reset Start-up Parameters responses - see Section 43.9.4
For further information on Commissioning cluster events, refer to Section 43.6.
Parent topic:Structures