BDB_tsOobReadDataToAuthenticate
The following structure contains data values that are read from the local node during out-of-band commissioning of the node.
typedef struct{
uint8 au8Key[16]__attribute__((aligned(16)));
uint64 u64TcAddress;
uint64 u64PanId;
uint16 u16ShortPanId;
uint8 u8ActiveKeySeq;
uint8 u8Channel;
}BDB_tsOobReadDataToAuthenticate;
where:
au8Key[16]__attribute__((aligned (16)))is an array containing the current network key, with one byte per array element.u64TcAddressis the IEEE/MAC address of the Trust Centre of the network to which the node is being commissioned.u64PanIdis the Extended PAN ID of the network to which the node is being commissioned.u16ShortPanIdis the PAN ID of the network to which the node is being commissioned.u8ActiveKeySeqis the key sequence number of the currently active network key.u8Channelis the radio channel number on which the network operates.
Parent topic:Structures