BDB_teCommissioningStatus
The following enumerations are used to indicate the status of the commissioning process for the node.
typedef enum
{
E_BDB_COMMISSIONING_STATUS_SUCCESS,
E_BDB_COMMISSIONING_STATUS_IN_PROGRESS,
E_BDB_COMMISSIONING_STATUS_NOT_AA_CAPABLE,
E_BDB_COMMISSIONING_STATUS_NO_NETWORK,
E_BDB_COMMISSIONING_STATUS_FORMATION_FAILURE,
E_BDB_COMMISSIONING_STATUS_NO_IDENTIFY_QUERY_RESPONSE,
E_BDB_COMMISSIONING_STATUS_BINDING_TABLE_FULL,
E_BDB_COMMISSIONING_STATUS_NO_SCAN_RESPONSE,
E_BDB_COMMISSIONING_STATUS_NOT_PERMITTED,
E_BDB_COMMISSIONING_STATUS_TCLK_EX_FAILURE
}BDB_teCommissioningStatus;
The enumerations are listed and described in the table below:
Commissioning Status Enumerations
Enumeration |
Description |
|---|---|
E_BDB_COMMISSIONING_STATUS_SUCCESS |
Commissioning is successfully completed |
E_BDB_COMMISSIONING_STATUS_IN_PROGRESS |
Commissioning is on-going |
E_BDB_COMMISSIONING_STATUS_NOT_AA_CAPABLE |
Parent cannot assign address to joining node |
E_BDB_COMMISSIONING_STATUS_NO_NETWORK |
No network is found that can be joined |
E_BDB_COMMISSIONING_STATUS_FORMATION_FAILURE |
Network formation failed |
E_BDB_COMMISSIONING_STATUS_NO_IDENTIFY_QUERY _ RESPONSE |
No responses received to an Identify Query command |
E_BDB_COMMISSIONING_STATUS_BINDING_TABLE_FULL |
The local Binding table is full |
E_BDB_COMMISSIONING_STATUS_NO_SCAN_RESPONSE |
No responses received during a channel scan |
E_BDB_COMMISSIONING_STATUS_NOT_PERMITTED |
Requested commissioning is not permitted |
E_BDB_COMMISSIONING_STATUS_TCLK_EX_FAILURE |
Trust Centre link key exchange failed |
Parent topic:Enumerations