ZPS_tsInterPanAddress
This structure is used to specify the destination for an inter-PAN transmission. The ZPS_tsInterPanAddressstructure is detailed below.
typedef struct
{
enum {
ZPS_E_AM_INTERPAN_GROUP = 0x01,
ZPS_E_AM_INTERPAN_SHORT,
ZPS_E_AM_INTERPAN_IEEE
}eMode;
uint16 u16PanId;
ZPS_tuAddress uAddress;
} ZPS_tsInterPanAddress;
where:
eModeis used to specify the type of destination address that will be used in the fielduAddressbelow. One of the following enumerations must be specified:ZPS_E_AM_INTERPAN_GROUPindicates that a 16-bit group address will be used to specify multiple target nodes in the destination network (the group address must be valid in the destination network)ZPS_E_AM_INTERPAN_SHORTindicates that a 16-bit network/short address will be used to specify a single target node or a broadcast to all nodes in the destination networkZPS_E_AM_INTERPAN_IEEEindicates that a 64-bit IEEE/MAC address will be used to specify a single target node in the destination network
u16PanIdis the PAN ID of the destination network - a value 0xFFFF can be used to specify a broadcast to all reachable ZigBee PRO networksuAddressis the address of the target node(s) in the destination network (the address type must be as specified above in theeModefield) - a value of 0xFFFF can be used to specify a broadcast to all nodes in the destination network(s).
Parent topic:Other structures