ZPS_tsAplZdpSimpleDescRsp
This structure is used to store Simple_Desc_rsp message data - a response to a call to the function ZPS_eAplZdpSimpleDescRequest(). This response contains the Simple descriptor of a given endpoint on the node with a given network address.
The ZPS_tsAplZdpSimpleDescRspstructure is detailed below.
typedef struct {
uint8 u8Status;
uint16 u16NwkAddrOfInterest;
uint8 u8Length;
/* Rest of the message is variable length */
ZPS_tsAplZdpSimpleDescType sSimpleDescriptor;
} ZPS_tsAplZdpSimpleDescRsp;
where:
u8Statusis the return status for ZPS_eAplZdpSimpleDescRequest().u16NwkAddrOfInterestis the network address of the remote node that sent the response (this is the network address that was specified in the request).u8Lengthis the length of the returned Simple descriptor, in bytes (depends on the number of clusters supported by the endpoint).sSimpleDescriptoris the returned Simple descriptor, a structure of typeZPS_tsAplZdpSimpleDescType(detailed in Section 9.2.1.3). This is only included ifu8Statusreports success.
Parent topic:ZDP response structures