ZPS_tsAplZdpPowerDescStoreRsp
This structure is used to store Power_Desc_store_rsp message data - a response to a call to the function ZPS_eAplZdpPowerDescStoreRequest(). This response indicates whether the sending node has successfully stored the received Power descriptor in its primary discovery cache.
The ZPS_tsAplZdpPowerDescStoreRspstructure is detailed below.
typedef struct {
uint8 u8Status;
uint64 u64IeeeAddr;
/* Rest of message is variable length */
ZPS_tsAplZdpNodePowerDescriptor sPowerDescriptor;
} ZPS_tsAplZdpPowerDescStoreRsp;
where:
u8Statusis the return status for ZPS_eAplZdpPowerDescStoreRequest().u64IeeeAddris the IEEE/MAC address of the device whose Power descriptor has been stored in the primary discovery cache.sPowerDescriptoris the Power descriptor stored (see Section 9.2.1.1).
Parent topic:ZDP response structures