ZPS_tsAplZdpPowerDescRsp
This structure is used to store Power_Desc_rsp message data - a response to a call to the function ZPS_eAplZdpPowerDescRequest(). This response contains the Power descriptor of the node with a given network address.
The ZPS_tsAplZdpPowerDescRspstructure is detailed below.
typedef struct {
uint8 u8Status;
uint16 u16NwkAddrOfInterest;
/* Rest of the message is variable length */
ZPS_tsAplZdpNodePowerDescriptor sPowerDescriptor;
} ZPS_tsAplZdpPowerDescRsp;
where:
u8Statusis the return status for ZPS_eAplZdpPowerDescRequest()u16NwkAddrOfInterestis the network address of the remote node that sent the response (this is the network address that was specified in the request)sPowerDescriptoris the returned Power descriptor, a structure of typeZPS_tsAplZdpNodePowerDescriptor(detailed in Section 9.2.1.2). This is only included ifu8Statusreports success
Parent topic:ZDP response structures