ZPS_tsAplZdpMgmtNwkDiscRsp
This structure is used to store Mgmt_NWK_Disc_rsp message data - a response to a call to the function ZPS_eAplZdpMgmtNwkDiscRequest(). This response reports the networks discovered in a network discovery (all the networks or a subset).
The ZPS_tsAplZdpMgmtNwkDiscRspstructure is detailed below.
typedef struct {
uint8 u8Status;
uint8 u8NetworkCount;
uint8 u8StartIndex;
uint8 u8NetworkListCount;
/* Rest of the message is variable length */
ZPS_tsAplZdpNetworkDescr* psNetworkDescrList;
} ZPS_tsAplZdpMgmtNwkDiscRsp;
where:
u8Statusis the return status for ZPS_eAplZdpMgmtNwkDiscRequest()u8NetworkCountis the total number of networks discoveredu8StartIndexis the index, in the complete list of discovered networks, of the first network reported in this response (throughpsNetworkDescrList)u8NetworkListCountis the number of discovered networks reported in this response (throughpsNetworkDescrList)psNetworkDescrListis a pointer to the first entry in a list of network descriptors for the discovered networks. Each entry is of the typeZPS_tsAplZdpNetworkDescrdetailed below.ZPS_tsAplZdpNetworkDescr
typedef struct { uint64 u64ExtPanId; uint8 u8LogicalChan; uint8 u8StackProfile; uint8 u8ZigBeeVersion; uint8 u8PermitJoining; uint8 u8RouterCapacity; uint8 u8EndDeviceCapacity; } ZPS_tsAplZdpNetworkDescr;
where:
u64ExtPanIdis the 64-bit extended PAN ID of the discovered network.u8LogicalChanis the radio channel in which the discovered network operates (value in range 0 to 26, but only channels 11 to 26 relevant to 2400-MHz band).u8StackProfileis the 4-bit identifier of the ZigBee stack profile used by the discovered network (0 - manufacturer-specific, 1 - ZigBee, 2 - ZigBee PRO, other values reserved) and is fixed at 2 for the NXP stack.u8ZigBeeVersionis the 4-bit version of the ZigBee protocol used by the discovered network.u8PermitJoiningindicates whether the discovered network is currently allowing joinings - that is, at least one node (a Router or the Coordinator) of the network is allowing other nodes to join it:0x01: Joinings allowed.
0x00: Joinings not allowed.
All other values reserved.
u8RouterCapacityindicates whether the device is capable of accepting join requests from Routers - set to TRUE if capable, FALSE otherwise.u8EndDeviceCapacityindicates whether the device is capable of accepting join requests from End Devices - set to TRUE capable, FALSE otherwise.
Parent topic:ZDP response structures