ZPS_tsAplZdpMgmtCacheRsp
This structure is used to store Mgmt_Cache_rsp message data - a response to a call to the function ZPS_eAplZdpMgmtCacheRequest(). This response reports a list of the End Devices registered in the node’s primary discovery cache.
The ZPS_tsAplZdpMgmtCacheRspstructure is detailed below.
typedef struct {
uint8 u8Status;
uint8 u8DiscoveryCacheEntries;
uint8 u8StartIndex;
uint8 u8DiscoveryCacheListCount;
/* Rest of the message is variable length */
ZPS_tsAplDiscoveryCache* pDiscoveryCacheList;
} ZPS_tsAplZdpMgmtCacheRsp;
where:
u8Statusis the return status for ZPS_eAplZdpMgmtCacheRequest()u8DiscoveryCacheEntriesis the total number of discovery cache entries on the remote node.u8StartIndexis the discovery cache index of the first entry reported in this response (throughpDiscoveryCacheList).u8DiscoveryCacheListCountis the number of discovery cache entries reported in this response (throughpDiscoveryCacheList).pRoutingTableListis a pointer to the first entry in the list of reported discovery cache entries. Each entry is of the typeZPS_tsAplDiscoveryCachedetailed below.
ZPS_tsAplDiscoveryCache
typedef struct {
uint64 u64ExtendedAddress;
uint16 u16NwkAddress;
} ZPS_tsAplDiscoveryCache;
where:
u64ExtendedAddressis the IEEE address of the End Device.u16NwkAddressis the network address of the End Device.
Parent topic:ZPS_tsAplZdpMgmtCacheRsp
Parent topic:ZDP response structures