ZPS_tsAplZdpMatchDescRsp
This structure is used to store Match_Desc_rsp message data - a response to a call to the function ZPS_eAplZdpMatchDescRequest(). This response contains details of the endpoints on the remote node that matched the criteria specified in the original request.
The ZPS_tsAplZdpMatchDescRspstructure is detailed below.
typedef struct {
uint8 u8Status;
uint16 u16NwkAddrOfInterest;
uint8 u8MatchLength;
/* Rest of message is variable length */
uint8* u8MatchList;
} ZPS_tsAplZdpMatchDescRsp;
where:
u8Statusis the return status for ZPS_eAplZdpMatchDescRequest().u16NwkAddrOfInterestis the network address of the remote node that sent the response (this is the network address that was specified in the request).u8MatchLengthis the length of the list of matched endpoints, in bytes.u8MatchListis a pointer to the list of matched endpoints, where each endpoint is represented by an 8-bit value (in the range 1-240).
Parent topic:ZDP response structures