ZPS_tsAplZdpFindNodeCacheReq
This structure is used by the function ZPS_eAplZdpActiveEpStoreRequest(). It represents a request to search for nodes in the network that hold ‘discovery information’ about a particular node.
The ZPS_tsAplZdpFindNodeCacheReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
} ZPS_tsAplZdpFindNodeCacheReq;
where:
u16NwkAddris the network address of the node of interestu64IeeeAddris the IEEE address of the node of interest
Parent topic:ZDP Request structures