ZPS_tsAplZdpExtendedActiveEpRsp
This structure is used to store Extended_Active_EP_rsp message data - a response to a call to the function ZPS_eAplZdpExtendedActiveEpRequest(). This response contains a list of the active endpoints on the node with a given network address.
The ZPS_tsAplZdpExtendedActiveEpRspstructure is detailed below.
typedef struct {
uint8 u8Status;
uint16 u16NwkAddr;
uint8 u8ActiveEpCount;
uint8 u8StartIndex;
/* Rest of the message is variable Length */
uint8* pActiveEpList;
} ZPS_tsAplZdpExtendedActiveEpRsp;
where:
u8Statusis the return status for ZPS_eAplZdpExtendedActiveEpRequest().16NwkAddris the network address of the remote node that sent the response (this is the network address that was specified in the request).u8ActiveEpCountis the total number of active endpoints on the node.u8StartIndexis the index, in the node’s list of active endpoints, of the first endpoint reported in this response.pActiveEpListis a pointer to the reported list of active endpoints (starting with the endpoint with indexu8StartIndex).
Parent topic:ZDP response structures