ZPS_tsAfZdoBindEvent
This structure is used in the ZPS_EVENT_ZDO_BIND event, which indicates that the local node has been successfully bound to one or more remote nodes.
The ZPS_tsAfZdoBindEventstructure is detailed below.
typedef struct { ZPS_tuAddress uDstAddr; uint8 u8DstAddrMode; uint8 u8SrcEp; uint8 u8DstEp; } ZPS_tsAfZdoBindEvent;
where
uDstAddris the address of the remote node for the binding (the type of address is specified using the elementu8DstAddrModeabove).u8DstAddrModeindicates the type of address specified through the elementuDstAddr(see Table 1).u8SrcEpis the number of the source endpoint for the binding (in range 1-240).u8DstEpis the number of the destination endpoint for the binding (in range 1-240).
Parent topic:Event structures