ZPS_tsAfNwkStatusIndEvent
This structure is used in the ZPS_EVENT_NWK_STATUS_INDICATION event, which reports status information from the NWK layer of the stack.
The ZPS_tsAfNwkStatusIndEventstructure is detailed below.
typedef struct {
uint16 u16NwkAddr;
uint8 u8Status;
} ZPS_tsAfNwkStatusIndEvent;
where:
u16NwkAddris the 16-bit network address of the node associated with the event.u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.
Parent topic:Event structures