ZPS_tsAfNwkJoinFailedEvent
This structure is used in the event ZPS_EVENT_NWK_FAILED_TO_JOIN, which indicates that the local device has failed to join a network.
The ZPS_tsAfNwkJoinFailedEventstructure is detailed below.
typedef struct
{
uint8 u8Status;
bool_t bRejoin;
} ZPS_tsAfNwkJoinFailedEvent;
where:
u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.bRejoinindicates whether the join attempt was a rejoin (TRUE) or a new association (FALSE).
Parent topic:Event structures