ZPS_tsAfNwkDiscoveryEvent
This structure is used in the ZPS_EVENT_NWK_DISCOVERY_COMPLETE event, which reports the details of the networks detected in a network discovery initiated by a Router or End Device that needs to join a network.
The ZPS_tsAfNwkDiscoveryEventstructure is detailed below.
typedef struct
{
uint32 u32UnscannedChannels;
uint8 eStatus;
uint8 u8NetworkCount;
uint8 u8SelectedNetwork;
ZPS_tsNwkNetworkDescr *psNwkDescriptors;
} ZPS_tsAfNwkDiscoveryEvent;
where:
u32UnscannedChannelsis a 32-bit bitmap representing the set of channels from the network discovery that had not yet been scanned when this event was generated. Bits 11 to 26 represent the 2400-MHz channels 11 to 26, where 1 indicates channel scanned and 0 indicates channel not yet scanned.estatusis the status of the network discovery process, returned by the lower layers (see Section 11.2) - MAC_ENUM_SUCCESS, if the discovery was successfully completed.u8NetworkCountis the number of networks that had been discovered when this event was generated.u8SelectedNetworkis the index of the recommended network in the array of reported networks (see below).psNwkDescriptorsis a pointer to the network discovery table in the network NIB. The network discovery table contains an array of data structures, where each structure contains details of a discovered network. Each array element is a structure of the typeZPS_tsNwkNetworkDescr, described in Section 8.2.3.1. The number of array elements is given byu8NetworkCount, described above.
Parent topic:Event structures