AWS IoT Device Shadow library
The AWS IoT Device Shadow library enables you to store and retrieve the current state (the “shadow”) of every registered device. The device’s shadow is a persistent, virtual representation of your device that you can interact with from AWS IoT Core even if the device is offline. The device state is captured as its “shadow” within a JSON document. The device can send commands over MQTT to get, update and delete its latest state as well as receive notifications over MQTT about changes in its state. Each device’s shadow is uniquely identified by the name of the corresponding “thing”, a representation of a specific device or logical entity on the AWS Cloud. See Managing Devices with AWS IoT for more information on IoT “thing”. More details about AWS IoT Device Shadow can be found in AWS IoT documentation. This library is distributed under the MIT Open Source License.
Note: From v1.1.0 release onwards, you can used named shadow, a feature of the AWS IoT Device Shadow service that allows you to create multiple shadows for a single IoT device.
This library has gone through code quality checks including verification that no function has a GNU Complexity score over 8, and checks against deviations from mandatory rules in the MISRA coding standard. Deviations from the MISRA C:2012 guidelines are documented under MISRA Deviations. This library has also undergone both static code analysis from Coverity static analysis, and validation of memory safety through the CBMC automated reasoning tool.
See memory requirements for this library here.
AWS IoT Device Shadow v1.3.0 source code is part of the FreeRTOS 202210.00 LTS release.
AWS IoT Device Shadow v1.0.2 source code is part of the FreeRTOS 202012.00 LTS release.
AWS IoT Device Shadow Config File
The AWS IoT Device Shadow library exposes configuration macros that are required for building the library.
A list of all the configurations and their default values are defined in shadow_config_defaults.h.
To provide custom values for the configuration macros, a custom config file named shadow_config.h can be provided by the user application to the library.
By default, a shadow_config.h custom config is required to build the library. To disable this requirement
and build the library with default configuration values, provide SHADOW_DO_NOT_USE_CUSTOM_CONFIG as a compile time preprocessor macro.
Building the Library
The shadowFilePaths.cmake file contains the information of all source files and the header include path required to build the AWS IoT Device Shadow library.
As mentioned in the previous section, either a custom config file (i.e. shadow_config.h) OR the SHADOW_DO_NOT_USE_CUSTOM_CONFIG macro needs to be provided to build the AWS IoT Device Shadow library.
For a CMake example of building the AWS IoT Device Shadow library with the shadowFilePaths.cmake file, refer to the coverity_analysis library target in test/CMakeLists.txt file.
Building Unit Tests
Checkout CMock Submodule
By default, the submodules in this repository are configured with update=none in .gitmodules to avoid increasing clone time and disk space usage of other repositories (like amazon-freertos that submodules this repository).
To build unit tests, the submodule dependency of CMock is required. Use the following command to clone the submodule:
git submodule update --checkout --init --recursive --test/unit-test/CMock
Platform Prerequisites
For building the library, CMake 3.13.0 or later and a C90 compiler.
For running unit tests, Ruby 2.0.0 or later is additionally required for the CMock test framework (that we use).
For running the coverage target, gcov and lcov are additionally required.
Steps to build unit tests
Go to the root directory of this repository. (Make sure that the CMock submodule is cloned as described above.)
Run the cmake command:
cmake -S test -B buildRun this command to build the library and unit tests:
make -C build allThe generated test executables will be present in
build/bin/testsfolder.Run
cd build && ctestto execute all tests and view the test run summary.
CBMC
To learn more about CBMC and proofs specifically, review the training material here.
The test/cbmc/proofs directory contains CBMC proofs.
In order to run these proofs you will need to install CBMC and other tools by following the instructions here.
Reference examples
Please refer to the demos of the AWS IoT Device Shadow library in the following locations for reference examples on POSIX and FreeRTOS platforms:
Platform |
Location |
Transport Interface Implementation |
|---|---|---|
POSIX |
POSIX sockets for TCP/IP and OpenSSL for TLS stack |
|
FreeRTOS |
FreeRTOS+TCP for TCP/IP and mbedTLS for TLS stack |
|
FreeRTOS |
Based on Secure Sockets Abstraction |
Documentation
Existing Documentation
For pre-generated documentation, please see the documentation linked in the locations below:
Location |
|---|
Note that the latest included version of IoT Device Shadow library may differ across repositories.
Generating documentation
The Doxygen references were created using Doxygen version 1.9.2. To generate the Doxygen pages, please run the following command from the root of this repository:
doxygen docs/doxygen/config.doxyfile
Contributing
See CONTRIBUTING.md for information on contributing.