usb_pd_alt_mode_dp_dock
Overview
This PD example is a simple demonstration based on the MCUXpresso SDK PD stack.
 The application use the shield dock board (om13790dock) to implement the DisplayPort alternate mode.
It recognize attached video source (like: “the shield host board (om13790host)” or “PC”), and drive the displayer to work.
System Requirement
Hardware requirements
One Type-C shield dock board
One 9V DC power supply
Type-C Cable
One hardware for a specific device, for example: one lpcxpresso54114 board
Personal Computer or the shield host board (om13790host)
Software requirements
The project files are in:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_pd_alt_mode_dp_dock/ / . 
The
is Bare Metal or FreeRTOS OS. 
Terminal tool.
Getting Started
Hardware Settings
 For detailed instructions, see the appropriate board User’s Guide.
Please reference to the re-worked document for hardware settings.
Prepare the example
For MCUXpresso, please reference to the MCUXpresso SDK USB Type-C PD Stack User’s Guide to make sure the SDK_DEBUGCONSOLE = 1 in project settings.
Download the program to the target board.
Power on shield dock board then power on development board.
Run the example
Download this program to the board.
Connect the displayer to the MinDP port (J2).
Connect one video source (like: “the shield host board (om13790host)” or “PC”) to the Type-C port (J1). For example: if the video source is PC, connect the shield dock board to PC with one Type-C cable.
The video source will recognize the shield dock board and the displayer works.
Supported Boards
LPCXpresso55S69