Hardware requirements
Type-C USB cable
FRDM-MCXL255 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a Type-C USB cable between the host PC and the MCU-Link USB port (J16) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the GLIKEY driver demo in the terminal window:
GLIKEY Peripheral Driver Example
*Success* GLIKEY is not locked
*Success* GLIKEY Sync Reset done
*Success* GLIKEY Start enable done
*Success* GLIKEY Continue enable Step 1 pass
*Success* GLIKEY Continue enable Step 2 pass
*Success* GLIKEY Continue enable Step 3 pass
*Success* GLIKEY Continue enable Step Enable pass
SUCCESS: Register on index 2 can be now written!
*Success* GLIKEY End of operation done
End of example