Build an example application

Perform the following steps to build the hello_world example application.

  1. Open the desired demo application workspace. Most example application workspace files can be located using the following path:

    <install_dir>/boards/<board_name>/<example_type>/<application_name>/iar
    

    Using the i.MX 93 AUTO EVK hardware platform as an example, the hello_world workspace is located in:

    <install_dir>/boards/mcimx93autoevk/demo_apps/hello_world/iar/hello_world.eww
    

    Other example applications may have additional folders in their path.

  2. Select the desired build target from the drop-down menu.

    For this example, select hello_world – debug.

    |

|

  1. To build the demo application, click Make, highlighted in red in Figure 2.

    |

|

  1. The build completes without errors.

Parent topic:Run a demo application using IAR