Summary of serial interface commands
The serial port connection to the Coordinator application is set up with the following configuration settings:
Baud rate = 115200
Data = 8 bits
Stop = 1 bit
Parity = None
The serial commands are not case-sensitive.
Serial command |
Action |
|---|---|
|
Sends an On/Off Toggle command to bound devices |
|
Triggers Network Steering for a device on the network |
|
Triggers network formation for a device not on a network |
|
Triggers Finding and Binding as an initiator |
|
Factory resets the device, erasing persistent data |
|
Triggers a software reset (no loss of data) |
Parent topic:Coordinator functionality