Bluetooth LE Shell
This section describes the functionality, user interactions, and testing methods for the Bluetooth LE Shell Application.
Implemented stack features
The Bluetooth LE Shell Application implements a console application that allows the user to interact with a full feature Bluetooth Low Energy stack library. It implements All GAP roles and both GATT client and server. Enabling these roles can be done using shell commands.
Parent topic:Bluetooth LE Shell
Implemented profile and services
The application implements a dynamic GATT database. The user can add services at runtime and also erase the database contents. The database is always populated with the GAP and GATT services. These services cannot be erased. The user can dynamically add the following services:
Heart Rate Service (UUID: 0x180D)
Battery Service (UUID: 0x180F)
Device Information Service (UUID: 0x180A)
Internet Support Profile Service (0x1820)
Parent topic:Bluetooth LE Shell
Supported platforms
The following platforms support the Bluetooth LE Shell application:
KW45B41Z-EVK
K32W148-EVK
FRDM-MCXW71
MCX-W71-EVK
KW47-EVK
FRDM-MCXW72
MCX-W72-EVK
Parent topic:Bluetooth LE Shell
User interface
After flashing the board, the device is in idle mode. The interaction with the board is done entirely by using the shell commands via the serial communication terminal.
Parent topic:Bluetooth LE Shell
Usage
The application is built to work with any other Bluetooth LE device. To showcase the functionality, two platforms are used in the following setup.
Open a serial port terminal and connect them to the two boards, in the same manner described in Testing devices. The start screen is displayed after the board is reset. All LEDs are flashing on both devices.
Configure one of the devices as a GAP peripheral and a Heart Rate server. Change name to HRS. Start advertising on this device.
BLE Shell>gap devicename HRS --> GATTDB Event: Attribute Written HRS>gap advdata 1 6 HRS>gap advdata 8 HRS HRS>gap advstart HRS> --> GAP Event: Advertising parameters successfully set. HRS> --> GAP Event: Advertising data successfully set. HRS> --> GAP Event: Advertising state changed successfully! HRS>gattdb addservice 0x180D --> Heart Rate - Heart Rate Measurement Value Handle: 14
Configure the other device as a GAP central. Change its name to ‘Collector’. Start scanning and connect to the HRS device by selecting the corresponding device index from the list of scanned devices. In the example below, the HRS device is device number 2. The number of listed scanned devices can be controller through the
mShellGapMaxScannedDevicesCount_cdefine inshell_gap.c.BLE Shell>gap devicename Collector --> GATTDB Event: Attribute Written Collector>gap scanstart filter --> GAP Event: Scan started. Collector> --> GAP Event: Found device 0 : 880F102F500E 0 dBm --> GAP Event: Found device 1 : NXP_CSCS 00049F000006 0 dBm --> GAP Event: Found device 2 : HRS 00049F0000FF 0 dBm Collector>gap connect 2 --> GAP Event: Scan stopped. Collector> --> GAP Event: Connected to peer 0
Optionally, the devices can be paired (gAppUsePairing_d and gAppUseBonding_d must be set in app_preinclude.h). On the collector initiate the pairing.
Collector>gap pair 0 --> Pairing... --> GAP Event: Link Encrypted --> GAP Event: Device Paired
On the Collector, start service discovery. The device discovers the GAP, GATT, and Heart Rate services.
Collector>gatt discover 0 -all --> Discovered primary services: 3 --> Generic Attribute Start Handle: 1 End Handle: 4 - Service Changed Value Handle: 3 - Client Characteristic Configuration Descriptor Handle: 4 --> Generic Access Start Handle: 5 End Handle: 11 - Device Name Value Handle: 7 - Appearance Value Handle: 9 - Peripheral Preferred Connection Parameters Value Handle: 11 --> Heart Rate Start Handle: 12 End Handle: 19 - Heart Rate Measurement Value Handle: 14 - Client Characteristic Configuration Descriptor Handle: 15 - Body Sensor Location Value Handle: 17 - Heart Rate Control Point Value Handle: 19
Configure the HRS to send notifications by writing the CCCD from the Collector. Send a GATT write command with value
1to the CCCD handle discovered, 15.Collector>gatt write 0 15 0x0001 --> GATT Event: Characteristic Value Written!
Send heart rate measurement notifications from the HRS device by using the value handle obtained after adding the service in the previous step.
HRS>gatt notify 0 14
A notification appears on the Collector console.
Collector> --> GATT Event: Received Notification Handle: 14 Value: B400
Extended advertising
Use the Bluetooth LE Shell application to exercise the advertising extension features:
On the GAP Peripheral device:
Configure the extended advertising parameters. In the below example, the advertising type is set to connectable and includes TX power and the primary PHY is set to Coded PHY.
Configure the extended advertising data. The Bluetooth LE Shell applications has the feature to send for test, a large data payload. Use the extended advertisement default configuration (not call “
gap extadvcfg”), pass the command “gap extadvdata” with no parameters and the default data is added. The length is configurable at compile time throughSHELL_EXT_ADV_DATA_SIZEand the data pattern isSHELL_EXT_ADV_DATA_PATTERN. Start the default test with call for “gap extadvstart”.The advertising data type is set to shortened local name (8) and the advertising data content is set to
test_ext_adv_data.Note: Users must note that extended connectable advertising does not allow for chained advertising data. The data length must be limited to what can fit in a single AUX_ADV_IND PDU (251 bytes at maximum). This means that passing the
gap extadvdatawith no parameters and the default value ofSHELL_EXT_ADV_DATA_SIZE(500 bytes) after having set the advertising type to connectable will result in an error when trying to start advertising.Start extended advertising.
BLE Shell>gap extadvcfg -type 65 -phy1 3 BLE Shell>gap extadvdata 8 test_ext_adv_data BLE Shell>gap extadvstart --> GAP Event: Extended Advertising parameters successfully set. --> GAP Event: Extended Advertising data successfully set. --> GAP Event: Advertising state changed successfully!
On the GAP Central device
Set the scanning parameters. The scanning PHY is set to match the advertising PHY, in this case Coded PHY.
Start scanning and filter duplicates.
BLE Shell>gap scancfg -phy 4 BLE Shell>gap scanstart filter BLE Shell> -> GAP Event: Scan started. BLE Shell> --> GAP Event: Found device 0 : 0060375BCEC6 -23 dBm Advertising Extended Data: test_ext_adv_data
Set the connection initiating PHYs corresponding to the primary PHY on which the advertising is performed.
Connect to the desired device in the scanned devices list.
BLE Shell>gap connectcfg -phy 4 --> Connection Parameters: --> Connection Interval: 200 ms --> Connection Latency: 0 --> Supervision Timeout: 32000 ms --> Connecting PHYs: Coded BLE Shell>gap connect 0 BLE Shell> -> GAP Event: Scan stopped. BLE Shell> --> GAP Event: Connected to peer 0
Parent topic:Usage
RSSI Monitor
RSSI Monitor is an application that allows monitoring the RSSI of a remote peer on advertising or connection channel. The GAP peripheral device can modify the output TX power on both advertising and connection channels.
On GAP peripheral device
Set the primary advertising PHY to Coded PHY. Start advertising and read the address. Set the TX power in dBm to a value less than 20 dBm.
BLE Shell>gap address BLE Shell> --> GAP Event: Public Address Read:C4603770BCC5 BLE Shell>gap extadvcfg -phy1 3 BLE Shell>gap extadvstart BLE Shell> --> GAP Event: Extended Advertising parameters successfully set. BLE Shell> --> GAP Event: Extended Advertising data successfully set. BLE Shell> --> GAP Event: Advertising state changed successfully! BLE Shell>gap txpower adv 0 BLE Shell> --> GAP Event: Success!
On GAP Central device
Set the scanning PHY to Coded PHY. Start monitoring the RSSI on advertising Channel using the address of the Peripheral device. Scanning starts automatically, if it is not previously enabled.
BLE Shell>gap scancfg -phy 4 BLE Shell>gap rssimonitor C4603770BCC5--> Reading RSSI on advertising channel: BLE Shell> -> GAP Event: Scan started. BLE Shell> RSSI: -27 dBm RSSI: -27 dBm RSSI: -27 dBm RSSI: -27 dBm RSSI: -27 dBm RSSI: -29 dBm
In the below example, the RSSI in monitored on a connection channel. On GAP Peripheral, start advertising in connectable mode on Coded PHY and adjust the TX power level.
BLE Shell>gap extadvcfg -type 65 -phy1 3 BLE Shell>gap extadvdata 8 rssimonitortest BLE Shell>gap extadvstart BLE Shell> --> GAP Event: Extended Advertising parameters successfully set. BLE Shell> --> GAP Event: Extended Advertising data successfully set. BLE Shell> --> GAP Event: Advertising state changed successfully! BLE Shell> --> GAP Event: Connected to peer 0 BLE Shell> --> GAP Event: Advertising stopped! BLE Shell>gap txpower conn 10 BLE Shell> --> GAP Event: Success!
On the GAP Central device, start scanning on the Coded PHY. Update the connection PHY also to Coded PHY, then connect to the remote device and monitor continuously the RSSI on the connection channel.
BLE Shell>gap scancfg -phy 4 BLE Shell>gap connectcfg -phy 4 --> Connection Parameters: --> Connection Interval: 200 ms --> Connection Latency: 0 --> Supervision Timeout: 32000 ms --> Connecting PHYs: Coded BLE Shell>gap scanstart filter BLE Shell> -> GAP Event: Scan started. BLE Shell> --> GAP Event: Found device 0 : C4603770BCC5 -21 dBm Advertising Extended Data: rssimonitortest gap connect 0 BLE Shell> -> GAP Event: Scan stopped. BLE Shell> --> GAP Event: Connected to peer 0 BLE Shell>gap rssimonitor 0 -c --> Reading RSSI from connected device: BLE Shell> RSSI: -22 dBm RSSI: -23 dBm RSSI: -21 dBm RSSI: -22 dBm RSSI: -22 dBm BLE Shell>gap rssistop
Update the PHY preference and continue monitoring the RSSI. For coded PHY, the coding scheme can be configured between S2 and S8 (500 kbit/s and 125 kbit/s).
BLE Shell>gap phy 0 -tx 4 -rx 4 -o 1 BLE Shell> --> GAP Event: Phy update complete with peer 0 --> TxPhy: Coded --> RxPhy: Coded BLE Shell>gap phy 0 -tx 2 -rx 2 BLE Shell> --> GAP Event: Phy update complete with peer 0 --> TxPhy: 2M --> RxPhy: 2M BLE Shell>gap rssimonitor 0 -c --> Reading RSSI from connected device: BLE Shell> RSSI: -23 dBm RSSI: -23 dBm RSSI: -21 dBm RSSI: -21 dBm --> GAP Event: Phy update complete with peer 0 --> TxPhy: Coded --> RxPhy: Coded BLE Shell> RSSI: -22 dBm RSSI: -21 dBm RSSI: -22 dBm RSSI: -23 dBm RSSI: -23 dBm --> GAP Event: Phy update complete with peer 0 --> TxPhy: 2M --> RxPhy: 2M BLE Shell> RSSI: -22 dBm RSSI: -21 dBm RSSI: -21 dBm RSSI: -20 dBm
Parent topic:Usage
Parent topic:Bluetooth LE Shell
Throughput feature
The Bluetooth LE Shell application also has a throughput test feature that can be used to test different combinations of the parameters (connection interval, payload size, and packet count) to determine the best data-rate.
This feature requires two devices:
GAP Peripheral: transmits the test packets
GAP Central: receives the packets and displays a report
All throughput-related commands are grouped under the **thrput** keyword:
thrput setparam: configures connection interval, packet count and payload size.thrput start tx: configures the device as a GAP Peripheral and starts advertising. Once the receiving device is connected, the packet transmission begins. The packet size and count can also be specified (-s<size_value>-c<count_value>).thrput start rx: configures the device as a GAP Central and starts scanning. Once a transmitter device is found, it connects to it and waits for the test to begin. The connection interval can also be configured (-ci<value>).thrput stop: stops the test and disconnects the devices.
Once a connection is established between the devices and initial throughput test is complete, one can start a new throughput transmission test with a new set of parameters (packet size / count).
The receiving device generates the report if no packets are received for more than three consecutive connection events.
The default configuration of the throughput test is the following:
Packet count: 1000
Payload size: 20 bytes
Connection interval (min, max): 160, 160 (200 ms)
The example of a test report is shown below:
BLE Shell>thrput start tx
BLE Shell>
--> GAP Event: Advertising parameters successfully set.
BLE Shell>
--> GAP Event: Advertising data successfully set.
BLE Shell>
--> GAP Event: Advertising started.
--> GAP Event: Connected to peer 0
BLE Shell>
--> GAP Event: Advertising Throughput test started.
Sending packets...
--> MTU Exchanged.
BLE Shell>
Throughput test with peer 0 has finished.
BLE Shell>thrput start rx
BLE Shell>
-> GAP Event: Scan started.
Found device:
THR_PER
0060375BCEC6
-> GAP Event: Scan stopped.
--> GAP Event: Connected to peer 0
BLE Shell>Throughput test started.
Receiving packets...
************************************
***** TEST REPORT FOR PEER ID 0 ****
************************************
Packets received: 1000
Total bytes: 244000
Receive duration: 5017 ms
Average bitrate: 389 kbps
************************************
********** END OF REPORT ***********
Parent topic:Bluetooth LE Shell
Decision-Based Advertising Filtering (DBAF) feature
The Bluetooth LE Shell application also supports the Decision-Based Advertising Filtering (DBAF) feature, which can be enabled by performing the following steps:
Flash the NBU: for KW45B41Z-EVK/K32W148-EVK/FRDM-MCXW71 flash the experimental NBU found in
middleware/wireless/ble_controller/bin/experimental; for KW47-EVK/MCX-W72-EVK/FRDM-MCXW72 flash the all-purpose NBU found inmiddleware/wireless/ble_controller/bin.Update the application project so that it uses the experimental Bluetooth LE Host library:
middleware/wireless/bluetooth/host/lib_exp/lib_ble_OPT_host_cm33_iar.aIn
app_preinclude.hfile, setBLE_SHELL_DBAF_SUPPORTto1.
This feature requires two devices:
GAP Peripheral: transmits decision PDUs (ADV_DECISION_IND).
GAP Central: scans for decision PDUs and handles filtering policies.
To showcase the functionality, two platforms are used in the following setup.
Steps to perform on the GAP Peripheral device:
Configure the extended advertising parameters to use decision PDUs. In the below example, the advertising type is set to connectable and includes TX power, uses decision PDUs and includes AdvA in the decision PDU. The primary PHY is set to Coded PHY.
Configure the extended advertising data using the
gap extadvdecdatacommand. The resolvable tag and/or arbitrary data can be set using the parameters available.Start extended advertising.
BLE Shell>gap extadvcfg -phy1 3 -type 449 BLE Shell>gap extadvdecdata -key 112233445566778899AABBCCDDEEFF00 -prand 5AC317 -decdata 6362 -datalen 2 -restag 0 BLE Shell>gap extadvstart BLE Shell> --> GAP Event: Extended Advertising parameters successfully set. BLE Shell> --> GAP Event: Extended Advertising data successfully set. BLE Shell> --> GAP Event: Extended Advertising Decision Data Setup Complete. BLE Shell> --> GAP Event: Advertising state changed successfully! BLE Shell>
Steps to perform on the GAP Central device:
Set the scanning parameters to scan only decision PDUs. The scanning PHY is set to match the advertising PHY, in this case Coded PHY.
Set the connection parameters to use only decision PDUs and the connection initiating PHYs corresponding to the primary PHY on which the advertising is performed.
BLE Shell>gap scancfg -phy 4 -filter 12 BLE Shell>gap connectcfg -phy 4 -filter 2 --> Connection Parameters: --> Connection Interval: 200 ms --> Connection Latency: 0 --> Supervision Timeout: 32000 ms --> Connecting PHYs: Coded --> Connection Filter Policy: 2 BLE Shell>
Add decision instructions using the
gap adddecinstrcommand. A maximum ofgMaxNumDecisionInstructions_cinstructions can be added. If the set of instructions must be changed, thegap deldecinstrcommand deletes all current instructions.BLE Shell>gap adddecinstr -group 1 -field 0 -criteria 1 -restagkey 112233445566778899AABBCCDDEEFF00 BLE Shell>gap adddecinstr -group 1 -field 6 -criteria 1 -advmode 6 BLE Shell>gap adddecinstr -group 0 -field 24 -criteria 1 -arbmask 00000000ffffff BLE Shell>gap adddecinstr -group 0 -field 9 -criteria 1 -advacheck 2 -add1type 0 -add1 a6fb0d376000 -add2type 0 -add2 a5fb0d376000 BLE Shell>gap adddecinstr -group 0 -field 7 -criteria 1 -rssimin -80 -rssimax 0 BLE Shell>gap adddecinstr -group 0 -field 8 -criteria 5 -lossmin 0 -lossmax 50 BLE Shell>
Set the decision instructions using the
gap setdecinstrcommand. The instructions are used when listening for advertisements containing decision PDUs.Start scanning and filter duplicates.
Connect to the desired device in the scanned devices list.
BLE Shell>gap setdecinstr BLE Shell> --> GAP Event: Decision Instructions Setup Complete. BLE Shell>gap scanstart filter BLE Shell> -> GAP Event: Scan started. BLE Shell> --> GAP Event: Found device 0 : C4603770BCC5 -23 dBm Advertising Extended Data: gap connect 0 BLE Shell> -> GAP Event: Scan stopped. BLE Shell> --> GAP Event: Connected to peer 0 BLE Shell>
Parent topic:Bluetooth LE Shell
Periodic Advertising with Responses (PAwR) feature
The Bluetooth LE Shell application also supports the Periodic Advertising with Responses feature, which can be enabled by performing the following steps:
Flash the NBU: for KW45B41Z-EVK/K32W148-EVK/FRDM-MCXW71 flash the experimental NBU found in
middleware/wireless/ble_controller/bin/experimental; for KW47-EVK/MCX-W72-EVK/FRDM-MCXW72 flash the all-purpose NBU found inmiddleware/wireless/ble_controller/bin.Update the application project so that it uses the experimental Bluetooth LE Host library,
middleware/wireless/bluetooth/host/lib_exp/lib_ble_OPT_host_cm33_iar.a.In
app_preinclude.hfile, setBLE_SHELL_PAWR_SUPPORTto1.
This feature requires two (or more) devices:
GAP Broadcaster: transmits advertising PDUs at a fixed interval. (AUX_SYNC_SUBEVENT_IND)
GAP Observer (one or more): scans for advertising PDUs and synchronizes with the advertising train. Sends responses PDUs in the synced subevents. (AUX_SYNC_SUBEVENT_RSP)
To showcase the functionality, two platforms are used in the following setup.
Steps to perform on the GAP Broadcaster device:
Configure the periodic advertising parameters. In the below example, a set of implicit values are used. There are 2 subevents per interval, each interval repeating at 1 second. There are 4 response slots configured per subevent, with the first response slot starting at 125ms from the advertising packet.
BLE Shell>gap periodiccfg --> Periodic Advertising Parameters: --> Periodic Advertising Handle: 1 --> Periodic Advertising Interval: 2000 ms --> Number of subevents: 2 --> Interval between subevents: 156.25 ms --> Time between the advertising packet in a subevent and the first response slot: 125.0 ms --> Time between response slots: 1.250 ms --> Number of response slots: 4 BLE Shell> --> GAP Event: Periodic Advertising parameters successfully set.
Alternatively, the command does accept all the mentioned parameters to be changed. The below command can be used to configure the exact same values.
BLE Shell>gap periodiccfg -numsubevents 2 -subint 125 -rspslotdelay 100 -rspslotspace 10 -numrspslot 4 BLE Shell> --> GAP Event: Periodic Advertising parameters successfully set.
Configure the subevent data on the advertiser for each subevent. Each instance of the
gap periodicsubeventdatacommand sets each subevent data for the configured number of subevents. In this used example, the first command sets the data for the first subevent, the second command sets the data for the second subevent. The upper limit is the lowest of the following:SHELL_PER_ADV_MAX_NUM_SUBEVENTSfromapp_preinclude.hor the number of subevents set usinggap periodiccfg.BLE Shell>gap periodicsubeventdata 255 696E666F31 BLE Shell>gap periodicsubeventdata 255 696E666F32
When the last subevent data is set, any succeeding command will erase the previously set data for all subevents, and the data in the ongoing command will be set in the first subevent.
Alternatively, the command accepts more advertising data structures for one subevent, up to
SHELL_EXT_ADV_DATA_MAX_AD_STRUCTURES.BLE Shell>gap periodicsubeventdata 27 01CAFECAFECAFE 255 696E666F31
To manually clear the data set for all the currently set subevents, you may issue the following command:
BLE Shell>gap periodicsubeventdata -erase
Start extended advertising.
BLE Shell>gap extadvstart BLE Shell> --> GAP Event: Extended Advertising parameters successfully set. BLE Shell> --> GAP Event: Extended Advertising data successfully set. BLE Shell> --> GAP Event: Advertising state changed successfully!
Start periodic advertising.
BLE Shell>gap periodicstart BLE Shell>Periodic Advertising state changed successfully!
Steps to perform on the GAP Observer device:
Start scanning using the
gap scanstartcommand. Optionally you can modify the scan parameters using thegap scancfgcommand.BLE Shell>gap scanstart BLE Shell> -> GAP Event: Scan started.
Issue a periodic sync command with the target address of the Broadcaster device that is periodic advertising. You can use the
gap addresscommand on the Broadcaster to obtain the address.BLE Shell>gap periodicsync -peer 006037A55E86
When the sync is established, events will be printed at the console.
--> GAP Event: Periodic Advertising Sync Established --> GAP Event: Periodic V2 Device Scanned Event Counter: 8 Subevent Synced: 0 RSSI: -38 dBm Advertising Data: info1
Synchronize the Observer device with the subevents needed. For this example, we will synchronize the Observer with both subevents using the following command. Implicitly, the Observer synchronizes to subevent 0.
BLE Shell>gap periodicsyncsubevent -peradvproperties 0 -numsubevents 2 -subevents 0x00,0x01 ... BLE Shell>Set Sync Subevent command successfully completed.
After this, GAP Events of type Periodic V2 Device Scanned should be displayed in the console for each of the subevents synchronized.
--> GAP Event: Periodic V2 Device Scanned Event Counter: 169 Subevent Synced: 0 RSSI: -34 dBm Advertising Data: info1 --> GAP Event: Periodic V2 Device Scanned Event Counter: 169 Subevent Synced: 1 RSSI: -38 dBm Advertising Data: info2
The last step to have a complete exchange of data is to set the response(s) on the Observer device. The next 2 commands will set the data for the 2 subevents synced at the previous step.
BLE Shell>gap periodicresponsedata -responsesubevent 0 -responseslot 0 -data 255 64657669636531696E666F31 BLE Shell>gap periodicresponsedata -responsesubevent 1 -responseslot 0 -data 255 64657669636531696E666F32
The
-responsesubeventparameter indicates the subevent the data is set for. The-responseslotparameter indicates the response slot the data is sent at this value should be within the range 0 to the number of response slots set atperiodiccfg.To scale the demo to use more Observer devices, repeat steps 1-3 for each of the added device. Also use example at step 4, with the adaptation of the
-responseslotaccording to the device index. The demo is designed to have a new device for each of the response slots available. Also, change the data to reflect the response of the extra device.Note: The
-dataparameter must be the last of theperiodicresponsedatacommand as it can contain a volatile number of advertising data structures.Alternatively, the command may contain additional advertising data structures.
BLE Shell>gap periodicresponsedata -responsesubevent 0 -responseslot 0 -data 27 01CAFECAFECAFE 255 64657669636531696E666F31 BLE Shell>gap periodicresponsedata -responsesubevent 1 -responseslot 0 -data 27 01CAFECAFECAFE 255 64657669636531696E666F32
To manually clear the data set for all the currently set subevents, you may issue the following command:
BLE Shell>gap periodicresponsedata -erase
Initiate a connection from PAwR
PAwR feature allows for connection initiation from the Broadcaster device. To do this, the devices have to be synchronized. The minimum steps required for this are steps 1, 3, 4 on the GAP Broadcaster device and steps 1, 2, GAP Observer device.
After performing the mentioned steps, the Broadcaster device must issue the following command:
BLE Shell>gap connectpawr -subevent 0 -peer 00603728063E -peeraddrtype 0
Upon successful connection the following message will be displayed.
--> GAP Event: Connected to peer 0
Parent topic:Bluetooth LE Shell
Parent topic:Bluetooth LE stack and demo applications