Changelog RPMSG-Lite
All notable changes to this project will be documented in this file.
The format is based on Keep a Changelog, and this project adheres to Semantic Versioning.
Unreleased
Added
Add MCXL20 porting layer and unit testing
New utility macro
RL_CALCULATE_BUFFER_COUNT_DOWN_SAFEto safely determine maximum buffer count within shared memory while preventing integer underflow.RT700 platform add support for MCMGR in DSPs
Changed
Change
rpmsg_platform.cto support new MCMGR APIImproved input validation in initialization functions to properly handle insufficient memory size conditions.
Refactored repeated buffer count calculation pattern for better code maintainability.
To make sure that remote has already registered IRQ there is required App level IPC mechanism to notify master about it
Fixed
Fixed CERT-C INT31-C violation by adding compile-time check to ensure
RL_PLATFORM_HIGHEST_LINK_IDremains within safe range for 16-bit casting in virtqueue ID creation.Fixed CERT-C INT30-C violations by adding protection against unsigned integer underflow in shared memory calculations, specifically in
shmem_length - (uint32_t)RL_VRING_OVERHEADandshmem_length - 2U * shmem_config.vring_sizeexpressions.Fixed CERT INT31-C violation in
platform_interrupt_disable()and similar functions by replacing unsafe cast fromuint32_ttoint32_twith a return of0constant.Fixed unsigned integer underflow in
rpmsg_lite_alloc_tx_buffer()where subtracting header size from buffer size could wrap around if buffer was too small, potentially leading to incorrect buffer sizing.Fixed CERT-C INT31-C violation in
rpmsg_lite.cwheresizeparameter was cast fromuint32_ttouint16_twithout proper validation.Applied consistent masking approach to both
sizeandflagsparameters:(uint16_t)(value & 0xFFFFU).This fix prevents potential data loss when size values exceed 65535.
Fixed CERT INT31-C violation in
env_memsetfunctions by explicitly convertingint32_tvalues to unsigned char using bit masking. This prevents potential data loss or misinterpretation when passing values outside the unsigned char range (0-255) to the standard memset() function.Fixed CERT-C INT31-C violations in RPMsg-Lite environment porting: Added validation checks for signed-to-unsigned integer conversions to prevent data loss and misinterpretation.
rpmsg_env_freertos.c: Added validation before converting int32_t to UBaseType_t.rpmsg_env_qnx.c: Fixed format string and added validation before assigning to mqstat fields.rpmsg_env_threadx.c: Added validation to prevent integer overflow and negative values.rpmsg_env_xos.c: Added range checking before casting to uint16_t.rpmsg_env_zephyr.c: Added validation before passing values to k_msgq_init.
Fixed a CERT INT31-C compliance issue in
env_get_current_queue_size()function where an unsigned queue count was cast to a signed int32_t without proper validation, which could lead to lost or misinterpreted data if queue size exceeded INT32_MAX.Fixed CERT INT31-C violation in
rpmsg_platform.cwherememcmp()return value (signed int) was compared with unsigned constant without proper type handling.Fixed CERT INT31-C violation in
rpmsg_platform.cwhere casting from uint32_t to uint16_t could potentially result in data loss. Changed length variable type from uint16_t to uint32_t to properly handle memory address differences without truncation.Fixed potential integer overflow in
env_sleep_msec()function in ThreadX environment implementation by rearranging calculation order in the sleep duration formula.Fixed CERT-C INT31-C violation in RPMsg-Lite where bitwise NOT operations on integer constants were performed in signed integer context before being cast to unsigned. This could potentially lead to misinterpreted data on
imx943platform.Added RL_MAX_BUFFER_COUNT (32768U) and RL_MAX_VRING_ALIGN (65536U) limit to ensure alignment values cannot contribute to integer overflow
Fixed CERT INT31-C violation in vring_need_event(), added cast to
uint16_tfor each operand.
5.1.4 - 27-Mar-2025
Added
Add KW43B43 porting layer
Changed
Doxygen bump to version 1.9.6
5.1.3 - 13-Jan-2025
Added
Memory cache management of shared memory. Enable with
#define RL_USE_DCACHE (1)inrpmsg_config.hin case of data cache is used.Cmake/Kconfig support added.
Porting layers for imx95, imxrt700, mcmxw71x, mcmxw72x, kw47b42 added.
5.1.2 - 08-Jul-2024
Changed
Zephyr-related changes.
Minor Misra corrections.
5.1.1 - 19-Jan-2024
Added
Test suite provided.
Zephyr support added.
Changed
Minor changes in platform and env. layers, minor test code updates.
5.1.0 - 02-Aug-2023
Added
RPMsg-Lite: Added aarch64 support.
Changed
RPMsg-Lite: Increased the queue size to (2 * RL_BUFFER_COUNT) to cover zero copy cases.
Code formatting using LLVM16.
Fixed
Resolved issues in ThreadX env. layer implementation.
5.0.0 - 19-Jan-2023
Added
Timeout parameter added to rpmsg_lite_wait_for_link_up API function.
Changed
Improved debug check buffers implementation - instead of checking the pointer fits into shared memory check the presence in the VirtIO ring descriptors list.
VRING_SIZE is set based on number of used buffers now (as calculated in vring_init) - updated for all platforms that are not communicating to Linux rpmsg counterpart.
Fixed
Fixed wrong RL_VRING_OVERHEAD macro comment in platform.h files
Misra corrections.
4.0.0 - 20-Jun-2022
Added
Added support for custom shared memory arrangement per the RPMsg_Lite instance.
Introduced new rpmsg_lite_wait_for_link_up() API function - this allows to avoid using busy loops in rtos environments, GitHub PR #21.
Changed
Adjusted rpmsg_lite_is_link_up() to return RL_TRUE/RL_FALSE.
3.2.0 - 17-Jan-2022
Added
Added support for i.MX8 MP multicore platform.
Changed
Improved static allocations - allow OS-specific objects being allocated statically, GitHub PR #14.
Aligned rpmsg_env_xos.c and some platform layers to latest static allocation support.
Fixed
3.1.2 - 16-Jul-2021
Added
Addressed MISRA 21.6 rule violation in rpmsg_env.h (use SDK’s PRINTF in MCUXpressoSDK examples, otherwise stdio printf is used).
Added environment layers for XOS.
Added support for i.MX RT500, i.MX RT1160 and i.MX RT1170 multicore platforms.
Fixed
Fixed incorrect description of the rpmsg_lite_get_endpoint_from_addr function.
Changed
Updated RL_BUFFER_COUNT documentation (issue #10).
Updated imxrt600_hifi4 platform layer.
3.1.1 - 15-Jan-2021
Added
Introduced RL_ALLOW_CONSUMED_BUFFERS_NOTIFICATION config option to allow opposite side notification sending each time received buffers are consumed and put into the queue of available buffers.
Added environment layers for Threadx.
Added support for i.MX8QM multicore platform.
Changed
Several MISRA C-2012 violations addressed.
3.1.0 - 22-Jul-2020
Added
Added support for several new multicore platforms.
Fixed
MISRA C-2012 violations fixed (7.4).
Fixed missing lock in rpmsg_lite_rx_callback() for QNX env.
Correction of rpmsg_lite_instance structure members description.
Address -Waddress-of-packed-member warnings in GCC9.
Changed
Clang update to v10.0.0, code re-formatted.
3.0.0 - 20-Dec-2019
Added
Added support for several new multicore platforms.
Fixed
MISRA C-2012 violations fixed, incl. data types consolidation.
Code formatted.
2.2.0 - 20-Mar-2019
Added
Added configuration macro RL_DEBUG_CHECK_BUFFERS.
Several MISRA violations fixed.
Added environment layers for QNX and Zephyr.
Allow environment context required for some environment (controlled by the RL_USE_ENVIRONMENT_CONTEXT configuration macro).
Data types consolidation.
1.1.0 - 28-Apr-2017
Added
Supporting i.MX6SX and i.MX7D MPU platforms.
Supporting LPC5411x MCU platform.
Baremental and FreeRTOS support.
Support of copy and zero-copy transfer.
Support of static API (without dynamic allocations).