Build an example application
Do the following steps to build the hello_world example application..
Open the desired demo application workspace. Most example application workspace files can be located using the following path:
<install_dir>/boards/<board_name>/<example_type>/<application_name>/iar
Using the
mcxw23evkhardware platform as an example, thehello_worldworkspace is located in:<install_dir>/boards/mcxw23evk/demo_apps/hello_world/iar/hello_world.eww
Other example applications may have additional folders in their path.
Select the desired build target from the drop-down menu.
For this example, select hello_world – debug.

To build the demo application, click Make, highlighted in red in Figure 2.

The build completes without errors.
Parent topic:Running a demo application using IAR