MCUXpresso SDK : mcuxsdk-middleware-erpc
Overview
This repository is for MCUXpresso SDK eRPC middleware delivery and it contains eRPC component officially provided in NXP MCUXpresso SDK. This repository is part of the MCUXpresso SDK overall delivery which is composed of several sub-repositories/projects. Navigate to the top/parent repository mcuxsdk for the complete delivery of MCUXpresso SDK to be able to build and run eRPC examples that are based on mcux-sdk-middleware-erpc component.
Documentation
Overall details can be reviewed here: MCUXpresso SDK Online Documentation
Visit eRPC - Documentation to review details on the contents in this sub-repo.
Setup
Instructions on how to install the MCUXpresso SDK provided from GitHub via west manifest Getting Started with SDK - Detailed Installation Instructions
Contribution
We welcome and encourage the community to submit patches directly to the eRPC project placed on github. Contributing can be managed via pull-requests. Before a pull-request is created the code should be tested and properly formatted.
eRPC
About
eRPC (Embedded RPC) is an open source Remote Procedure Call (RPC) system for multichip embedded systems and heterogeneous multicore SoCs.
Unlike other modern RPC systems, such as the excellent Apache Thrift, eRPC distinguishes itself by being designed for tightly coupled systems, using plain C for remote functions, and having a small code size (<5kB). It is not intended for high performance distributed systems over a network.
eRPC does not force upon you any particular API style. It allows you to export existing C functions, without having to change their prototypes. (There are limits, of course.) And although the internal infrastructure is written in C++, most users will be able to use only the simple C setup APIs shown in the examples below.
A code generator tool called erpcgen is included. It accepts input IDL files, having an .erpc extension, that have definitions of your data types and remote interfaces, and generates the shim code that handles serialization and invocation. erpcgen can generate either C/C++ or Python code.
Example .erpc file:
// Define a data type.
enum LEDName { kRed, kGreen, kBlue }
// An interface is a logical grouping of functions.
interface IO {
// Simple function declaration with an empty reply.
set_led(LEDName whichLed, bool onOrOff) -> void
}
Client side usage:
void example_client(void) {
erpc_transport_t transport;
erpc_mbf_t message_buffer_factory;
erpc_client_t client_manager;
/* Init eRPC client infrastructure */
transport = erpc_transport_cmsis_uart_init(Driver_USART0);
message_buffer_factory = erpc_mbf_dynamic_init();
client_manager = erpc_client_init(transport, message_buffer_factory);
/* init eRPC client IO service */
initIO_client(client_manager);
// Now we can call the remote function to turn on the green LED.
set_led(kGreen, true);
/* deinit objects */
deinitIO_client();
erpc_client_deinit(client_manager);
erpc_mbf_dynamic_deinit(message_buffer_factory);
erpc_transport_tcp_deinit(transport);
}
void example_client(void) {
erpc_transport_t transport;
erpc_mbf_t message_buffer_factory;
erpc_client_t client_manager;
/* Init eRPC client infrastructure */
transport = erpc_transport_cmsis_uart_init(Driver_USART0);
message_buffer_factory = erpc_mbf_dynamic_init();
client_manager = erpc_client_init(transport, message_buffer_factory);
/* scope for client service */
{
/* init eRPC client IO service */
IO_client client(client_manager);
// Now we can call the remote function to turn on the green LED.
client.set_led(kGreen, true);
}
/* deinit objects */
erpc_client_deinit(client_manager);
erpc_mbf_dynamic_deinit(message_buffer_factory);
erpc_transport_tcp_deinit(transport);
}
Server side usage:
// Implement the remote function.
void set_led(LEDName whichLed, bool onOrOff) {
// implementation goes here
}
void example_server(void) {
erpc_transport_t transport;
erpc_mbf_t message_buffer_factory;
erpc_server_t server;
erpc_service_t service = create_IO_service();
/* Init eRPC server infrastructure */
transport = erpc_transport_cmsis_uart_init(Driver_USART0);
message_buffer_factory = erpc_mbf_dynamic_init();
server = erpc_server_init(transport, message_buffer_factory);
/* add custom service implementation to the server */
erpc_add_service_to_server(server, service);
// Run the server.
erpc_server_run();
/* deinit objects */
destroy_IO_service(service);
erpc_server_deinit(server);
erpc_mbf_dynamic_deinit(message_buffer_factory);
erpc_transport_tcp_deinit(transport);
}
// Implement the remote function.
class IO : public IO_interface
{
/* eRPC call definition */
void set_led(LEDName whichLed, bool onOrOff) override {
// implementation goes here
}
}
void example_server(void) {
erpc_transport_t transport;
erpc_mbf_t message_buffer_factory;
erpc_server_t server;
IO IOImpl;
IO_service io(&IOImpl);
/* Init eRPC server infrastructure */
transport = erpc_transport_cmsis_uart_init(Driver_USART0);
message_buffer_factory = erpc_mbf_dynamic_init();
server = erpc_server_init(transport, message_buffer_factory);
/* add custom service implementation to the server */
erpc_add_service_to_server(server, &io);
/* poll for requests */
erpc_status_t err = server.run();
/* deinit objects */
erpc_server_deinit(server);
erpc_mbf_dynamic_deinit(message_buffer_factory);
erpc_transport_tcp_deinit(transport);
}
A number of transports are supported, and new transport classes are easy to write.
Supported transports can be found in erpc/erpc_c/transport folder. E.g:
CMSIS UART
NXP Kinetis SPI and DSPI
POSIX and Windows serial port
TCP/IP (mostly for testing)
SPIdev Linux
USB CDC
NXP Messaging Unit
eRPC is available with an unrestrictive BSD 3-clause license. See the LICENSE file for the full license text.
Releases
Edge releases
Edge releases can by found on eRPC CircleCI webpage. Choose build of interest, then platform target and choose ARTIFACTS tab. Here you can find binary application from chosen build.
Documentation
Documentation is in the wiki section.
Examples
Example IDL is available in the examples/ folder.
Plenty of eRPC multicore and multiprocessor examples can be also found in NXP MCUXpressoSDK packages. Visit https://mcuxpresso.nxp.com to configure, build and download these packages.
To get the board list with multicore support (eRPC included) use filtering based on Middleware and search for ‘multicore’ string. Once the selected package with the multicore middleware is downloaded, see
<MCUXpressoSDK_install_dir>/boards/<board_name>/multicore_examples for eRPC multicore examples (RPMsg_Lite or Messaging Unit transports used) or
<MCUXpressoSDK_install_dir>/boards/<board_name>/multiprocessor_examples for eRPC multiprocessor examples (UART or SPI transports used).
eRPC examples use the ‘erpc_’ name prefix.
Another way of getting NXP MCUXpressoSDK eRPC multicore and multiprocessor examples is using the mcux-sdk Github repo. Follow the description how to use the West tool to clone and update the mcuxsdk repo in readme Overview section. Once done the armgcc eRPC examples can be found in
mcuxsdk/examples/<board_name>/multicore_examples or in
mcuxsdk/examples/<board_name>/multiprocessor_examples folders.
You can use the evkmimxrt1170 as the board_name for instance. Similar to MCUXpressoSDK packages the eRPC examples use the ‘erpc_’ name prefix.
References
This section provides links to interesting erpc-based projects, articles, blogs or guides:
Directories
doc - Documentation.
doxygen - Configuration and support files for running Doxygen over the eRPC C++ infrastructure and erpcgen code.
erpc_c - Holds C/C++ infrastructure for eRPC. This is the code you will include in your application.
erpc_python - Holds Python version of the eRPC infrastructure.
erpcgen - Holds source code for erpcgen and makefiles or project files to build erpcgen on Windows, Linux, and OS X.
erpcsniffer - Holds source code for erpcsniffer application.
examples - Several example IDL files.
mk - Contains common makefiles for building eRPC components.
test - Client/server tests. These tests verify the entire communications path from client to server and back.
utilities - Holds utilities which bring additional benefit to eRPC apps developers.
Building and installing
These build instructions apply to host PCs and embedded Linux. For bare metal or RTOS embedded environments, you should copy the erpc_c directory into your application sources.
CMake and KConfig build:
It builds a static library of the eRPC C/C++ infrastructure, the erpcgen executable, and optionally the unit tests and examples.
CMake is compatible with gcc and clang. On Windows local MingGW downloaded by script can be used.
Make build:
It builds a static library of the eRPC C/C++ infrastructure, the erpcgen executable, and optionally the unit tests.
The makefiles are compatible with gcc or clang on Linux, OS X, and Cygwin. A Windows build of erpcgen using Visual Studio is also available in the erpcgen/VisualStudio_v14 directory. There is also an Xcode project file in the erpcgen directory, which can be used to build erpcgen for OS X.
Requirements
eRPC now support building erpcgen, erpc_lib, tests and C examples using CMake.
Requirements when using CMake:
CMake (minimal version 3.20.0)
Generator - Make, Ninja, …
C/C++ compiler - GCC, CLANG, …
Binson - https://www.gnu.org/software/bison/
Flex - https://github.com/westes/flex/
Requirements when using Make:
Make
C/C++ compiler - GCC, CLANG, …
Binson - https://www.gnu.org/software/bison/
Flex - https://github.com/westes/flex/
Windows
Related steps to build erpcgen using Visual Studio are described in erpcgen/VisualStudio_v14/readme_erpcgen.txt.
To install MinGW, Bison, Flex locally on Windows:
./install_dependencies.ps1
* ```
#### Linux
```bash
./install_dependencies.sh
Mandatory for case, when build for different architecture is needed
gcc-multilib, g++-multilib
Mac OS X
./install_dependencies.sh
Building
CMake and KConfig
eRPC use CMake and KConfig to configurate and build eRPC related targets. KConfig can be edited by prj.conf or menuconfig when building.
Generate project, config and build. In erpc/ execute:
cmake -B ./build # in erpc/build generate cmake project
cmake --build ./build --target menuconfig # Build menuconfig and configurate erpcgen, erpc_lib, tests and examples
cmake --build ./build # Build all selected target from prj.conf/menuconfig
**CMake will use the system’s default compilers and generator
If you want to use Windows and locally installed MinGW, use CMake preset :
cmake --preset mingw64 # Generate project in ./build using mingw64's make and compilers
cmake --build ./build --target menuconfig # Build menuconfig and configurate erpcgen, erpc_lib, tests and examples
cmake --build ./build # Build all selected target from prj.conf/menuconfig
Make
To build the library and erpcgen, run from the repo root directory:
make
To install the library, erpcgen, and include files, run:
make install
You may need to sudo the make install.
By default this will install into /usr/local. If you want to install elsewhere, set the PREFIX environment variable. Example for installing into /opt:
make install PREFIX=/opt
List of top level Makefile targets:
erpc: build the liberpc.a static libraryerpcgen: build the erpcgen toolerpcsniffer: build the sniffer tooltest: build the unit tests under the test directoryall: build all of the aboveinstall: install liberpc.a, erpcgen, and include files
eRPC code is validated with respect to the C++ 11 standard.
Installing for Python
To install the Python infrastructure for eRPC see instructions in the erpc python readme.
Known issues and limitations
Static allocations controlled by the ERPC_ALLOCATION_POLICY config macro are not fully supported yet, i.e. not all erpc objects can be allocated statically now. It deals with the ongoing process and the full static allocations support will be added in the future.
Code providing
Repository on Github contains two main branches: main and develop. Code is developed on develop branch. Release version is created via merging develop branch into main branch.
Copyright 2014-2016 Freescale Semiconductor, Inc.
Copyright 2016-2024 NXP