Hardware requirements
FRDM-MCXA276 board
USB-C cable
Personal Computer
Board settings
MCUBoot layout
Region |
From |
To |
Size |
|---|---|---|---|
MCUboot code |
0x00000000 |
0x00008000 |
32kB |
Primary slot |
0x00008000 |
0x0007DFFF |
472kB |
Secondary slot |
0x0007E000 |
0x000F3FFF |
472kB |
MCUBoot header size is set to 512 bytes
Signing algorithm is ECDSA-P256
Write alignment is 16 bytes
Uses image swapping by
SWAP_USING_MOVE
Image signing example
imgtool sign --key sign-ecdsa-p256-priv.pem
--align 16
--version 1.1
--slot-size 0x76000
--header-size 0x200
--pad-header
--max-sectors 59
ota_mcuboot_basic.bin
ota_mcuboot_basic.SIGNED.bin
If you experience problems with flash erase, check correct configuration
of ACL_SEC_x fields in CMPA region.