Hardware requirements
Type-C USB cable
FRDM-MCXA166 board
Personal Computer
Board settings
AOI_OUT = EXT_TRIG_OUT0 P1_2 J6-5 IO0 = EXT_TRIG_IN0 P1_0 J6-6 IO1 = EXT_TRIG_IN1 P1_1 J6-4
AOI_OUT = IO0 & IO1
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the aoi demo in the terminal window:
AOI_io_and project.
When IO0 and IO1 are both high level, the AOI_OUT is high level. When any of IO is low level, the AOI_OUT is low level.