Memory requirements
The following are the memory requirements for the SSRC module.
Memory item  | 
Size in bytes  | 
|---|---|
Instance memory (persistent)  | 
548  | 
Scratch memory (non-persistent)  | 
15.536 1  | 
Program memory for Arm9E and XScale  | 
14k  | 
Program memory for Arm7  | 
15k  | 
Parent topic:Resource usage
1 Worst case number for I/O buffers of 40 ms. If smaller I/O buffers are used, this number is smaller. The required scratch memory is roughly equal to 2 times the buffer size on the highest sample rate.