MCUXpresso SDK Release Notes
Overview
The MCUXpresso SDK is a comprehensive software enablement package designed to simplify and accelerate application development with Arm Cortex-M-based devices from NXP, including its general purpose, crossover and Bluetooth-enabled MCUs. MCUXpresso SW and Tools for DSC further extends the SDK support to current 32-bit Digital Signal Controllers. The MCUXpresso SDK includes production-grade software with integrated RTOS (optional), integrated enabling software technologies (stacks and middleware), reference software, and more.
In addition to working seamlessly with the MCUXpresso IDE, the MCUXpresso SDK also supports and provides example projects for various toolchains. The Development tools chapter in the associated Release Notes provides details about toolchain support for your board. Support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.
Underscoring our commitment to high quality, the MCUXpresso SDK is MISRA compliant and checked with Coverity static analysis tools. For details on MCUXpresso SDK, see MCUXpresso-SDK: Software Development Kit for MCUXpresso.
MCUXpresso SDK
As part of the MCUXpresso software and tools, MCUXpresso SDK is the evolution of Kinetis SDK, includes support for LPC, DSC,PN76, and i.MX System-on-Chip (SoC). The same drivers, APIs, and middleware are still available with support for Kinetis, LPC, DSC, and i.MX silicon. The MCUXpresso SDK adds support for the MCUXpresso IDE, an Eclipse-based toolchain that works with all MCUXpresso SDKs. Easily import your SDK into the new toolchain to access to all of the available components, examples, and demos for your target silicon. In addition to the MCUXpresso IDE, support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.
In order to maintain compatibility with legacy Freescale code, the filenames and source code in MCUXpresso SDK containing the legacy Freescale prefix FSL has been left as is. The FSL prefix has been redefined as the NXP Foundation Software Library.
Development tools
The MCUXpresso SDK is compiled and tested with these development tools:
IAR Embedded Workbench for Arm, version is 9.60.3
MCUXpresso IDE, Rev. 24.12
MCUXpresso for VS Code v24.12
GCC Arm Embedded Toolchain 13.2.1
Supported development systems
This release supports board and devices listed in following table. The board and devices in bold were tested in this release.
Development boards |
MCU devices |
|---|---|
KW47-EVK |
KW47B42Z83AFTA, KW47B42Z96AFTA, KW47B42Z97AFTA, |
MCUXpresso SDK release package
The MCUXpresso SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, CMSIS, devices, middleware, and RTOS support.
Device support
The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.
Board support
The boards folder provides the board-specific demo applications, driver examples, and middleware examples.
Demo application and other examples
The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.
RTOS
FreeRTOS
Real-time operating system for microcontrollers from Amazon
Middleware
Wireless Bluetooth LE host stack and applications
The Bluetooth LE Host Stack component provides an implementation for a Bluetooth LE mandatory and some optional, proprietary, and experimental features. The Bluetooth LE Host Stack component provides application examples, services, and profiles.
Main features supported:
Automotive Compliance
MISRA Compliance
HIS CCM <= 20
Advanced Secure Mode
Enhanced ATT
GATT Caching
Bluetooth LE Host GCC Libraries
Bluetooth LE Host IAR Libraries
Bluetooth LE Host Peripheral Libraries
Bluetooth LE Central Libraries
Bluetooth LE Host Full Host Features Libraries
Bluetooth LE Host Optional Features Libraries
Bluetooth LE Host Mandatory Features Libraries
Bare-metal and FreeRTOS Support
Bluetooth LE Privacy Support
CCC Sample Applications
Enhanced Notifications
Dynamic Database
OTA Support - Sample Applications
Decision based Advertising Filtering (DBAF) - Experimental feature
Advertising Coding Selection (ACS) - Experimental feature
Channel Sounding - Experimental feature with controlled access (contact your NXP representative for access)
Bluetooth LE Controller main and experimental features and capabilities described below are supported by the Bluetooth LE Host.
Note: For evaluating DBAF and ACS experimental features, replace the Bluetooth LE Host default example projects libraries with the libraries from the SDK folder ..\middleware\wireless\bluetooth\host\lib_exp and enable the features in the application. The Radio Subsystem (NBU) Firmware with experimental features is required.
Bluetooth LE Controller
Main features supported:
Peripheral Role
Central Role
Multiple PHYs (1 Mbps, 2 Mbps, Coded PHY)
Asymmetric Connections
Public/Random/Static Addresses
Network/Device Privacy Modes
Extended Advertising
Extended Scanning
Passive/Active Scanning
LE Encryption
LE Ping Procedure
HCI Test Interface
UART Test Interface
Randomized Advertising Channel Indexing
Sleep Clock Accuracy Update - Mechanism
ADI Field in Scan Response Data
HCI Support for Debug Keys in LE - Secure Connections
Main capabilities supported:
Simultaneous scanning 1 Mbps and Long Range
Scanning and advertising in parallel
24 connections as a central role
24 connections as a peripheral role
Any combination of central and peripheral roles (24 connections maximum)
8 connections with a 7.5 ms connection interval
Two advertising sets in parallel
26 Accept List entries
36 Resolvable Private Address (RPA) entries
Up to six Chain Packets per Extended Advertising set
Enhanced Notification on end of - Scanning/Advertising/Connection events
Connection event counters associated to Bluetooth LE packet reception
Timestamp associated to Bluetooth LE packet reception
RF channel info associated to Bluetooth LE packet reception
NXP proprietary Bluetooth LE Handover feature
Decision Based Advertising Filtering (DBAF) - Experimental feature. See Note below.
Advertising Coding Selection (ACS) - Experimental feature. See Note below.
Periodic Advertising with Responses (PAwR) - Experimental feature. See Note below. Additional features supported for KW47 and MCX W72 devices:
Channel Sounding - Experimental feature
Note: Project configuration enabling Experimental features on KW45 and MCX W71 requires the Radio Subsystem (NBU) Firmware to be reprogrammed with the firmware provided in the SDK under \middleware\wireless\ble_controller\bin\experimental\. For NBU programming steps, see the EVK Quick Start Guide and Secure Provisioning SDK (SPSDK) documentation.
Project configurations that require usage of the Bluetooth LE controller including all Bluetooth LE examples require the Radio Subsystem (NBU) Firmware to be re-programmed with the firmware provided in the SDK under middleware\wireless\ble_controller\bin.
GenFSK link layer
The Generic FSK protocol enables radio operation using a custom GFSK/GMSK or MSK modulation format.
Main Features supported:
Highly configurable packet structure
Optimized Sequence Command Set
High-precision timebase to maintain network timing
Two timer-compare mechanisms for Interrupt Generation and Sequence Launching
Hardware automation for packet transmit and receive, CRC and Whitening
Up to four network addresses to synchronize to, can be 8-bit, 16-bit or 32-bit
Packet Lengths up to 2047 Bytes
Support complex auto-sequence, like CCA before TX, Auto-ACK, TR.
Many operating modes can support the sending and receiving of multiple protocol packets, such as Bluetooth LE.
Wireless XCVR
The XCVR component provides a base Transceiver Driver for the 2.4 GHz narrowband radio.
Wireless Connectivity Framework
The Connectivity Framework is a software component that provides hardware abstraction modules to the upper layer connectivity stacks and components. It also provides a list of services and APIs, such as, Low power, Over the Air (OTA) Firmware update, File System, Security, Sensors, Serial Connectivity Interface (FSCI), and others. The Connectivity Framework modules are located in the middleware\wireless\framework SDK folder.
Wireless Low-power reference design applications (central and peripheral)
The Low-Power Reference Design Applications provide reference design source code and projects showcasing how to implement optimized low power functionality based on a Bluetooth LE application. For additional details, see the readme.md.
CMSIS DSP Library
The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.
NXP PSA CRYPTO DRIVER
PSA crypto driver for crypto library integration via driver wrappers
EdgeLock SE050 Plug and Trust Middleware
Secure subsystem library - SSS APIs
Multicore
Multicore Software Development Kit
mbedTLS
mbedtls SSL/TLS library v3.x
mbedTLS
mbedtls SSL/TLS library v2.x
LittleFS
LittleFS filesystem stack
LIN Stack
LIN Stack middleware
FreeMASTER
FreeMASTER communication driver for 32-bit platforms.
Release contents
Provides an overview of the MCUXpresso SDK release package contents and locations.
Deliverable |
Location |
|---|---|
Boards |
INSTALL_DIR/boards |
Demo Applications |
INSTALL_DIR/boards/<board_name>/demo_apps |
Driver Examples |
INSTALL_DIR/boards/<board_name>/driver_examples |
eIQ examples |
INSTALL_DIR/boards/<board_name>/eiq_examples |
Board Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/boards/<board_name>/project_template |
Driver, SoC header files, extension header files and feature header files, utilities |
INSTALL_DIR/devices/<device_name> |
CMSIS drivers |
INSTALL_DIR/devices/<device_name>/cmsis_drivers |
Peripheral drivers |
INSTALL_DIR/devices/<device_name>/drivers |
Toolchain linker files and startup code |
INSTALL_DIR/devices/<device_name>/<toolchain_name> |
Utilities such as debug console |
INSTALL_DIR/devices/<device_name>/utilities |
Device Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/devices/<device_name>/project_template |
CMSIS Arm Cortex-M header files, DSP library source |
INSTALL_DIR/CMSIS |
Components and board device drivers |
INSTALL_DIR/components |
RTOS |
INSTALL_DIR/rtos |
Release Notes, Getting Started Document and other documents |
INSTALL_DIR/docs |
Tools such as shared cmake files |
INSTALL_DIR/tools |
Middleware |
INSTALL_DIR/middleware |
What is new
The following changes have been implemented compared to the previous SDK release version (25.03.00-pvw2).
Bluetooth LE host stack and applications
Added
L2CAP support for Channel Sounding IQ Sample Transfer in CCC CS sample applications.
Changed
Updated FSCI XML file.
Updated Bluetooth LE Host Documentation.
Fixed
Cleared the mpRemoteCachedCaps entry when the peer disconnects (CS sample applications).
Transfer RAS subscription data during connection handover (CCC CS sample applications).
EAD - Updated advertising data length check to ensure encrypted data fits inside one AD.
Updated digital_key_car_anchor and digital_key_car_anchor_cs applications to manage Random Static address from the application layer.
Details can be found in CHANGELOG.md.
Bluetooth LE controller
HADM, PAwR, DBAF fixes and stability improvements.
Transceiver drivers (XCVR)
Added support for Bluetooth LE Channel Sounding
Added API to control PA ramp type and duration
Connectivity framework
Minor Changes (no impact on application)
General
[General] Various MISRA/Coverity fixes in framework: NVM, RNG, LowPower, SecLib and platform files
Services
[SecLib_RNG] fix return status from RNG_GetTrueRandomNumber() function: return correctly gRngSuccess_d when RNG_entropy_func() function is successful
[SFC] Allow the application to override the trig sample number parameter
[Settings] Re-define the framework settings API name to avoid double definition when gSettingsRedefineApiName_c flag is defined
Platform specific
[wireless_mcu] fwk_platform_sensors update :
Enable temperature measurement over ADC ISR
Enable temperature handling requested by NBU
[kw47_mcxw72] Change the default ppm_target of SFC algorithm from 200 to 360ppm
Details can be found in CHANGELOG.md
Known issues
This section lists the known issues, limitations, and/or workarounds.
New project wizard compile failure
The following components request the user to manually select other components that they depend upon in order to compile. These components depend on several other components and the New Project Wizard (NPW) is not able to decide which one is needed by the user.
Note: xxx means core variants, such as, cm0plus, cm33, cm4, cm33_nodsp.
Also for low-level adapter components, currently the different types of the same adapter cannot be selected at the same time. For example, if there are two types of timer adapters, gpt_adapter and pit_adapter, only one can be selected as timer adapter in one project at a time. Duplicate implementation of the function results in an error.
Only FreeRTOS is tested for RTOS support
This release only supports the FreeRTOS kernel and a bare-metal non-preemptive task scheduler.
Disabled pairing and bonding for most sensor applications
Most sensor applications have pairing and bonding disabled to allow a faster interaction with mobile applications. These two security features can be enabled in the app_preinclude.h header file.
Bluetooth LE
Most sensor applications have pairing and bonding disabled to allow a faster interaction with mobile applications. These two security features can be enabled in the app_preinclude.h header file.
Bluetooth LE controller:
Max number of connections supported : 8
Potential instabilities particularly with short Connection Intervals
Channel Sounding (CS) not supported:
RTT with Random sequence
RTT Random sequence NADM
TX SNR
LE 2M 2BT PHY
More than one CS procedure in parallel
Potential instabilities with small CS offset or small subevent interval
TQI not accurate
Periodic Advertising with Responses (PAwR):
Incorrect data in Periodic Advertising Response is reported if AUX_SYNC_SUBEVENT_RSP contained an extended header.
Sync device cannot synchronize on more than 32 subevents.
Connection establishment using PAwR in LE Coded PHY can potentially fail.
Data report can potentially be truncated on the first AUX_ADV_IND of an extended advertising train containing an ACAD field.
Other limitations
The following Connectivity Framework configurations are Experimental and not recommended for mass production:
Power down on application power domain.
XTAL32K less board with FRO32K support.
FRO32K notifications callback is for debug only. Application shall not execute long processing (such as PRINTF) as it is executed in ISR context.
A hardfault can be encountered when using fsl_component_mem_manager_light.c memory allocator and shutting down some unused RAM banks in low power. It is due to a wrong reinitialization of ECC RAM banks. To be sure not to reproduce the issue,
gPlatformShutdownEccRamInLowPowershould be set to 0.GenFSK
Connectivity_testapplication is not operational with Low Power enabled.Serial manager is only supported on UART (not I2C nor SPI).
The
--no-warn-rwx-segmentscannot been recognized on legacy MCUXpresso IDE versions.The
--no-warn-rwx-segmentsoption in MCUXpresso projects should be manually removed from the project settings if someone needs to use legacy (< 11.8.0) MCUXpresso IDE versionsIf the FRO32K is configured as the clock source of the CM33 Core then the debug session will block in both IAR, MCUX CMSIS-DAP while debugging. Use a lower debug wire speed, for example 1 MHz instead of the default one.
In IAR, the option is in Runtime Checking -> Debugger -> CMSIS DAP -> Interface -> Interface speed.
In MCUXpresso IDE, the option is in LinkServer Debugger -> Advanced Settings -> Wirespeed (Hz).
Low power reference design applications are not supported for the armgcc toolchain from zip archives. Please use MCUXpresso IDE or IAR toolchains for development using these applications.
Latest MCUX IDE 24.9.25 cannot support KW47 multicore compiling
The latest MCUX IDE 24.9.25 cannot support KW47 multicore compiling, users need to upgrade to the Linkserver_24.10.22 or higher version, and change the LinkServer path configuration in the MCUX IDE. Two ways to change the LinkerSever path in the MCUX IDE.
Option 1 (recommended): Using the custom Path

Option 2: Using the command-line to change the settings
Close the MCUXpresso IDE if it is open.
Execute the following command:
<path_to_MCUXpressoIDE_installation_folder>\ide\mcuxpressoide -application com.nxp.mcuxpresso.headless.application -nosplash -run set.config.preference com.nxp.mcuxpresso.core.debug.support.linkserver:linkserver.path.default_path=<path_to_LinkServer_installation_folder>
where:
<path_to_MCUXpressoIDE_installation_folder>is the folder where the MCUXpresso IDE is installed.<path_to_LinkServer_installation_folder>is the folder where the new/custom LinkServer is installed.
Example:
C:\NXP\MCUXpressoIDE_24.9.25\ide\mcuxpressoide -application com.nxp.mcuxpresso.headless.application -nosplash -run set.config.preference com.nxp.mcuxpresso.core.debug.support.linkserver:linkserver.path.default_path=c:\NXP\LinkServer_24.10.15
Examples hello_world_ns, secure_faults_ns, and secure_faults_trdc_ns have incorrect library path in GUI projects
When the affected examples are generated as GUI projects, the library linking the secure and non-secure worlds has an incorrect path set. This causes linking errors during project compilation.
Examples: hello_world_ns, hello_world_s, secure_faults_ns, secure_faults_s, secure_faults_trdc_ns, secure_faults_trdc_s
Affected toolchains: mdk, iar
Workaround: In the IDE project settings for the non-secure (_ns) project, find the linked library (named hello_world_s_CMSE_lib.o, or similar, depending on the example project) and replace the path to the library with <build_directory>/<secure_world_project_folder>/<IDE>/, replacing the subdirectory names with the build directory, the secure world project name, and IDE name.