Introduction
This branch contains unified IPv4 and IPv6 functionalities. Refer to the Getting started Guide (found here) for more details.
FreeRTOS-Plus-TCP Library
FreeRTOS-Plus-TCP is a lightweight TCP/IP stack for FreeRTOS. It provides a familiar Berkeley sockets interface, making it as simple to use and learn as possible. FreeRTOS-Plus-TCP’s features and RAM footprint are fully scalable, making FreeRTOS-Plus-TCP equally applicable to smaller lower throughput microcontrollers as well as larger higher throughput microprocessors.
This library has undergone static code analysis and checks for compliance with the MISRA coding standard. Any deviations from the MISRA C:2012 guidelines are documented under MISRA Deviations. The library is validated for memory safety and data structure invariance through the CBMC automated reasoning tool for the functions that parse data originating from the network. The library is also protocol tested using Maxwell protocol tester for both IPv4 and IPv6.
Getting started
The easiest way to use the 4.0.0 version of FreeRTOS-Plus-TCP is to refer the Getting started Guide (found here) Another way is to start with the pre-configured demo application project (found in this directory). That way you will have the correct FreeRTOS source files included, and the correct include paths configured. Once a demo application is building and executing you can remove the demo application files, and start to add in your own application source files. See the FreeRTOS Kernel Quick Start Guide for detailed instructions and other useful links.
Additionally, for FreeRTOS-Plus-TCP source code organization refer to the Documentation, and API Reference.
Getting help
If you have any questions or need assistance troubleshooting your FreeRTOS project, we have an active community that can help on the FreeRTOS Community Support Forum. Please also refer to FAQ for frequently asked questions.
Also see the Submitting a bugs/feature request section of CONTRIBUTING.md for more details.
Note: All the remaining sections are generic and applies to all the versions from V3.0.0 onwards.
Upgrading to V3.0.0 and V3.1.0
In version 3.0.0 or 3.1.0, the folder structure of FreeRTOS-Plus-TCP has changed and the files have been broken down into smaller logically separated modules. This change makes the code more modular and conducive to unit-tests. FreeRTOS-Plus-TCP V3.0.0 improves the robustness, security, and modularity of the library. Version 3.0.0 adds comprehensive unit test coverage for all lines and branches of code and has undergone protocol testing, and penetration testing by AWS Security to reduce the exposure to security vulnerabilities. Additionally, the source files have been moved to a source directory. This change requires modification of any existing project(s) to include the modified source files and directories. There are examples on how to use the new files and directory structure. For an example based on the Xilinx Zynq-7000, use the code in this branch and follow these instructions to build and run the demo.
FreeRTOS-Plus-TCP V3.1.0 source code(.c .h) is part of the FreeRTOS 202210.00 LTS release.
Generating pre V3.0.0 folder structure for backward compatibility:
If you wish to continue using a version earlier than V3.0.0 i.e. continue to use your existing source code organization, a script is provided to generate the folder structure similar to this.
Note: After running the script, while the .c files will have same names as the pre V3.0.0 source, the files in the include directory will have different names and the number of files will differ as well. This should, however, not pose any problems to most projects as projects generally include all files in a given directory.
Running the script to generate pre V3.0.0 folder structure: For running the script, you will need Python version > 3.7. You can download/install it from here.
Once python is downloaded and installed, you can verify the version from your terminal/command window by typing python --version.
To run the script, you should switch to the FreeRTOS-Plus-TCP directory that was created using the Cloning this repository step above.
And then run python <Path/to/the/script>/GenerateOriginalFiles.py.
To consume FreeRTOS+TCP
Consume with CMake
If using CMake, it is recommended to use this repository using FetchContent.
Add the following into your project’s main or a subdirectory’s CMakeLists.txt:
Define the source and version/tag you want to use:
FetchContent_Declare( freertos_plus_tcp
GIT_REPOSITORY https://github.com/FreeRTOS/FreeRTOS-Plus-TCP.git
GIT_TAG master #Note: Best practice to use specific git-hash or tagged version
GIT_SUBMODULES "" # Don't grab any submodules since not latest
)
Configure the FreeRTOS-Kernel and make it available
this particular example supports a native and cross-compiled build option.
set( FREERTOS_PLUS_FAT_DEV_SUPPORT OFF CACHE BOOL "" FORCE)
# Select the native compile PORT
set( FREERTOS_PLUS_FAT_PORT "POSIX" CACHE STRING "" FORCE)
# Select the cross-compile PORT
if (CMAKE_CROSSCOMPILING)
# Eg. Zynq 2019_3 version of port
set(FREERTOS_PLUS_FAT_PORT "ZYNQ_2019_3" CACHE STRING "" FORCE)
endif()
FetchContent_MakeAvailable(freertos_plus_tcp)
Consuming stand-alone
This repository uses Git Submodules to bring in dependent components.
Note: If you download the ZIP file provided by GitHub UI, you will not get the contents of the submodules. (The ZIP file is also not a valid Git repository)
To clone using HTTPS:
git clone https://github.com/FreeRTOS/FreeRTOS-Plus-TCP.git ./FreeRTOS-Plus-TCP
cd ./FreeRTOS-Plus-TCP
git submodule update --checkout --init --recursive tools/CMock test/FreeRTOS-Kernel
Using SSH:
git clone git@github.com:FreeRTOS/FreeRTOS-Plus-TCP.git ./FreeRTOS-Plus-TCP
cd ./FreeRTOS-Plus-TCP
git submodule update --checkout --init --recursive tools/CMock test/FreeRTOS-Kernel
Porting
The porting guide is available on this page.
Repository structure
This repository contains the FreeRTOS-Plus-TCP repository and a number of supplementary libraries for testing/PR Checks. Below is the breakdown of what each directory contains:
tools
This directory contains the tools and related files (CMock/uncrustify) required to run tests/checks on the TCP source code.
tests
This directory contains all the tests (unit tests and CBMC) and the dependencies (FreeRTOS-Kernel/Litani-port) the tests require.
source/portable
This directory contains the portable files required to compile the FreeRTOS-Plus-TCP source code for different hardware/compilers.
source/include
The include directory has all the ‘core’ header files of FreeRTOS-Plus-TCP source.
source
This directory contains all the [.c] source files.
Note
At this time it is recommended to use BufferAllocation_2.c in which case it is essential to use the heap_4.c memory allocation scheme. See memory management.
Kernel sources
The FreeRTOS Kernel Source is in FreeRTOS/FreeRTOS-Kernel repository, and it is consumed by testing/PR checks as a submodule in this repository.
The version of the FreeRTOS Kernel Source in use could be accessed at ./test/FreeRTOS-Kernel directory.
CBMC
The test/cbmc/proofs directory contains CBMC proofs.
To learn more about CBMC and proofs specifically, review the training material here.
In order to run these proofs you will need to install CBMC and other tools by following the instructions here.