Running the A2B scenario
The A2B feature allows for the secure transfer of Bluetooth Low Energy security keys information between the Car Anchor devices. The feature is currently supported on the following platforms:
KW45B41Z-EVK with a lifecycle state of OEM-Open or higher, this feature is provided by the EdgeLock Secure Enclave.
KW47-EVK with a lifecycle state of OEM-Open or higher, this feature is provided by th EdgeLock Secure Enclave.
The Car Anchor demo application makes use of the A2B feature to securely synchronize the local IRK and the Bonding Data (LTK and peer IRK) with another Car Anchor.
Prerequisites:
Three boards (two act as Car Anchors, one as a Device). The demo is currently limited to a maximum of two Car Anchors.
The two Car Anchors must be connected via a serial interface as described in the section above.
Advanced Secure Mode must be enabled. The following macros must be defined and set to
1in*app\_preinclude.h*for the digital_key_car_anchor project:gAppSecureMode_dgA2BEnabled_d
One of the Car Anchors must be configured with the
*gA2BInitiator\_d*macro set to1, this is called Car Anchor A, and the other must be configured with the*gA2BInitiator\_d*macro set to0, called Car Anchor B. Car Anchor A triggers the EdgeLock-to-EdgeLock (E2E) key derivation and local IRK synchronization. Therefore, it should be started up after Car Anchor B.
Demo steps:
Start Car Anchor B, then Car Anchor A. At initialization the E2E key is derived and the local IRK of Car Anchor A is sent as a secure blob to Car Anchor B in order for both Car Anchors to have the same local IRK as shown in the Figure 1 and Figure 2.


Trigger the Owner Pairing scenario by sending the “
sd” command on the Device and “sd op” on Car Anchor A. Once the bond is created, the Bonding Data containing secured blobs for the LTK and peer IRK is sent to Car Anchor B. The Car Anchors display the Bonding Data in shell with the LTK in blob form (the LTK is never available in plain text) and the peer IRK in plain text. Now both Car Anchors have the same Bonding Data. Refer Figure 3 and Figure 4.

Disconnect Car Anchor A by sending the “
dcnt” command.Once Car Anchor A is disconnected, send “
sd” on the Device and “sd pe” on Car Anchor B. Car Anchor B is now able to perform a Passive Entry connection, without pairing as shown in Figure 5.