Feature enable and memory impact

Features

Macros to enable the feature

Memory impact

CSI

CONFIG_CSI

Flash - 60K, RAM - 4K

DPP

CONFIG_WPA_SUPP_DPP

Flash - 240K, RAM - 12K

Independent reset

CONFIG_WIFI_IND_DNLD
CONFIG_WIFI_IND_RESET

Minimal

Parallel firmware download Wi-Fi

CONFIG_WIFI_IND_DNLD

Minimal

Parallel firmware download Bluetooth

CONFIG_BT_IND_DNLD

Minimal

WPA3 enterprise

CONFIG_WPA_SUPP_CRYPTO_ENTERPRISE [Macros specific to EAP-methods included]
CONFIG_EAP_TLS
CONFIG_EAP_PEAP
CONFIG_EAP_TTLS
CONFIG_EAP_FAST
CONFIG_EAP_SIM
CONFIG_EAP_AKA
CONFIG_EAP_AKA_PRIME

Flash - 165K, RAM - 18K

WPA2 enterprise

CONFIG_WPA_SUPP_CRYPTO_ENTERPRISE [Macros specific to EAP-methods included]
CONFIG_EAP_TLS
CONFIG_EAP_PEAP
CONFIG_EAP_TTLS
CONFIG_EAP_FAST
CONFIG_EAP_SIM
CONFIG_EAP_AKA
CONFIG_EAP_AKA_PRIME

Flash - 165K, RAM - 18K

Host sleep

CONFIG_HOST_SLEEP

Minimal

WMM

CONFIG_WMM[^1]

Flash - 10K, RAM - 57K

802.11mc

CONFIG_11MC
CONFIG_CSI
CONFIG_WLS_CSI_PROC[^2]
CONFIG_11AZ

Flash: 52.78KB, RAM : 121.1KB

802.11az

CONFIG_11MC
CONFIG_CSI[2]
CONFIG_WLS_CSI_PROC[^2]
CONFIG_11AZ

Flash: 52.78KB, RAM : 121.1KB

Non-blocking firmware download mechanism

CONFIG_FW_DNLD_ASYNC

—

Note:

  • For Wi-Fi, the macros are set with the value “0” by default in the file wifi_config_default.h located in <SDK_PATH>/middleware/wifi_nxp/incl/ directory.

    To enable the features, set the value of the macros to “1*” in the file wifi_config.h located in*<SDK_Wi-Fi_Example_PATH>/ directory***.***

  • Bluetooth

    To enable the features, set the value of the macros to “1” in the file app_bluetooth_config.h located in <SDK_Bluetooth_Example_PATH>/ directory.

SLIM feature

The SLIM feature is used to reduce the consumption of the flash memory and SRAM of low-end boards like the FRDM MCXN947.

Memory impact:

  • Maximum Flash usage: 607.62 KB (29.67%).

  • Maximum SRAM usage: 297.73 KB (58.15%)

SLIM macros

Feature disabled

CONFIG_WIFI_SLIM_ROAM

CONFIG_ROAMING
CONFIG_11K
CONFIG_11V
CONFIG_11R

CONFIG_WIFI_SLIM_STA

CONFIG_5GHz_SUPPORT\ (applicable for RW612)
CONFIG_CLOUD_KEEP_ALIVE
CONFIG_WIFI_EU_CRYPTO
CONFIG_TX_AMPDU_PROT_MODE
CONFIG_WNM_PS CONFIG_TURBO_MODE
CONFIG_AUTO_RECONNECT
CONFIG_DRIVER_OWE CONFIG_OWE
CONFIG_WIFI_FORCE_RTS
CONFIG_WIFI_FRAG_THRESHOLD
CONFIG_COMBO_SCAN
CONFIG_SCAN_CHANNEL_GAP

CONFIG_WIFI_SLIM_UAP

CONFIG_UAP_STA_MAC_ADDR_FILTER
CONFIG_WIFI_MAX_CLIENTS_CNT

CONFIG_FREERTOS_LOW_MEMORY_FOOTPRINT

When the macro is enabled, the heap memory usage is reduced by 10 KB (from 70 KB to 60 KB).

CONFIG_LWIP_LOW_MEM_FOOTPRINT

When the macro is enabled:

  • The memory usage is reduced by curtailing LWIP stack parameters.
  • The data throughput is reduced.
  • Data net-stats are disabled.

Parent topic:Feature enable and memory impact

[^1] The macro is not used for IW416.

[^2] Prerequisite macros for 802.11mc and 802.11az features