Hardware
Because USB Type-C PD stack needs one provider and one consumer, the demo hardware needs two of the same set of devices; a development board and shield board, shield host board or shield dock board. For example, the LPCXpresso54114 and USB-PD/Type C shield board.
|
|
|
|
Supported boards list
FRDM-K22F Rev A
FRDM-K64F Rev C
FRDM-KL27Z Rev A
FRDM-KL28Z Rev A
FRDM-KL32L2A4S Rev A
IMXRT1050-EVKB
LPCXpresso54018 Rev D
LPCXpresso54114 Rev A
LPCXpresso54608 Rev B
LPCXpresso55S16 Rev A
LPCXpresso55S28 Rev A1
LPCXpresso55S69 Rev 1
MIMXRT1015-EVK Rev A
MIMXRT1020-EVK
MIMXRT1040-EVK
MIMXRT1050-EVK
MIMXRT1060-EVK
MIMXRT1064-EVK
MIMXRT1170-EVK Rev B
MIMXRT685-EVK Rev E
MC56F83000-EVK
MIMXRT1060-EVKB
MIMXRT1160-EVK
MIMXRT595-EVK
LPCXpresso55S36
MIMXRT685-AUD-EVK
MIMXRT1170-EVKB
Parent topic:Hardware
Hardware re-work
The following table provides information regarding I2C selection.
| |I2C_0|I2C_1|
|::|:—–:|:—–:|
|FRDM-K22F||√|
|FRDM-K64F|√||
|FRDM-KL27Z|√||
|FRDM-KL28Z||√|
|FRDM-KL32L2A4S| |√|
|IMXRT1050-EVKB||√|
|LPCXpresso54018|√||
|LPCXpresso54114|√||
|LPCXpresso54608|√||
|LPCXpresso55S16|√||
|LPCXpresso55S28|√||
|LPCXpresso55S69|√||
|MIMXRT1015-EVK|√||
|MIMXRT1020-EVK|√||
|MIMXRT1040-EVK|√| |
|MIMXRT1050-EVK||√|
|MIMXRT1060-EVK|√||
|MIMXRT1064-EVK|√||
|MIMXRT1170-EVK|√||
|MIMXRT685-EVK|√||
|MC56F83000-EVK|√||
|MIMXRT1060-EVKB|√| |
|MIMXRT1160-EVK|√| |
|MIMXRT595-EVK|√| |
|LPCXpresso55S36|√| |
|MIMXRT685-AUD-EVK|√| |
|MIMXRT1170-EVKB|√| |
Note:
For om13588, I2C_0 means placing 1-2 for jumper J11 and J12.
For om13588, I2C_1 means placing 2-3 for jumper J11 and J12.
For om13790host and om13790dock, I2C_0 means placing 1-2 for jumper J14 and J15.
For om13790host and om13790dock, I2C_1 means placing 2-3 for jumper J14 and J15.
LCPXpresso55S28: None {#GUID-55FB7531-3AC6-4817-869A-82A9BF9DAC37 .section}
The connection state is as follows:
|
|
LPCXpresso54114: None {#GUID-C17E255B-BDB5-4D82-A022-3DC3530647D6 .section}
The connection state is as follows:
|
|
LPCXpresso54018 and LPCXpresso54608: {#GUID-95D1B63B-5C9E-4E6F-A74E-3937BA9892ED .section}
Connect the USBPD-C-SHIELD board to the Arduino headers in the LPCXpresso54608 evaluation board.
The PTN5110 interrupt signal (nALERT) is connected to the Arduino D4 pin receptacle. The software architecture requires nALERT to be routed to an interrupt enabled IO. The LPCXpresso54608 D4 input pin PIO4_7 does not have interrupt functionality.
To work around this, use a blue wire connection between J404-1 and J403-8 for shield board om13588, between J9-1 and J6-8 for shield host board om13790host to use the PIO1_22 interrupt capable input.
The connection state is as follows:
|
|
LPCXpresso55S69: None {#GUID-555587E0-AF00-4CA4-B127-B43B0FFCF9DF .section}
The connection state is as follows:
|
|
FRDM-KL27Z: None {#GUID-FD35582C-C265-42CA-8CC3-C9560F178E06 .section}
The connection state is as follows:
|
|
FRDM-K22F: None {#GUID-D8BF3371-9166-49CA-87B6-56847BDAF86D .section}
|
|
FRDM-K64F: None {#GUID-1D85BD62-E0F5-4F47-BBF1-2AAE596C3DB6 .section}
|
|
FRDM-KL28Z: None {#GUID-9C554B54-C266-4735-A9C3-457E08E8E95E .section}
The connection state is as follows:
|
|
MIMXRT1050-EVK and IMXRT1050-EVKB: None {#GUID-F092A7C0-D752-4FE4-B125-6F0BCD2EFB21 .section}
The connection state is as follows:
|
|
MIMXRT1020-EVK: None {#GUID-C66FEEBF-20B9-40B3-B377-6CF518F027AD .section}
The connection state is as follows:
|
|
MIMXRT1060-EVK: None {#GUID-A9B337EC-5065-4AFD-B637-4AFCD3A16C9C .section}
The connection state is as follows:
|
|
MIMXRT1064-EVK: None {#GUID-3E88740D-BDF3-4968-8946-EB1A4688F550 .section}
The connection state is as follows:
|
|
Note: Before powering up, verify the USB Type-C shield is pushed all the way into the Arduino header with good contact. Make sure there are no unintentional shorts (like jumper, blue wires) between the USB Type-C Shield board and the main development board.
MIMXRT685-EVK: None {#GUID-8E4B171A-BDF1-4DE5-B3B0-7CA7DBDECF9D .section}
The connection state is as follows:
|
|
MIMXRT1015-EVK: None {#GUID-8B9270E6-AC70-4D85-89E9-937801295648 .section}
The connection state is as follows:
|
|
MIMXRT1170-EVK: None {#GUID-4612B680-76C1-4B81-923C-C8EAB43C4763 .section}
The connection state is as follows:
|
|
FRDM-KL32L2A4S: None {#GUID-47EEF23B-9A4E-4692-B317-B2A48325736B .section}
The connection state is as follows:
|
|
LPCXpresso55S16: None {#GUID-68703EDB-541A-47A3-BB0B-EFEF9E046947 .section}
The connection state is as follows:
|
|
MC56F83000-EVK: None {#GUID-6B058003-4590-4CC0-A9B3-ECC0B78ADE2D .section}
The connection state is as follows:
|
|
MIMXRT1060-EVKB: None {#GUID-BAD .section}
The connection state is as follows:
|
|
MIMXRT1160-EVK: None {#GUID-117F .section}
The connection state is as follows:
|
|
MIMXRT595-EVK: None {#GUID-059D .section}
The connection state is as follows:
|
|
LPCXpresso55S36: None {#GUID-059D2 .section}
The connection state is as follows:
|
|
MIMXRT685-AUD-EVK: None {#GUID-9BA108DC-9FFF-4D86-85D3-B64DBB1B5CF2 .section}
The connection state is as follows:
|
|
Parent topic:Hardware