Hardware requirements
Micro USB cable
FRDM-KE15Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Press the reset button to begin running the demo.
Running the demo
Disconnect any debugger to run this demo in case the sequence of entering sleep mode is interrupted. When the example runs successfully, you can see the similar information from the terminal as below.
LPI2C_VLPS demo start...
X:    2,  Y: -148,  Z: 2107
X:   -2,  Y:  -97,  Z: 2086