Software Component
Componentization
To improve software component integration and portability, all MCUXpresso SDK components including drivers, components, utilities and middlewares are recorded and used in a componentized way instead of fragment code lines.
In addition to the sources, one software component always contains CMakeLists.txt and Kconfig files. CMake part defines the sources, includes, static configurations, versions, etc while Kconfig part defines the dynamic configurations and dependencies.
CMakeLists.txt
In CMakeLists.txt, component data shall be recorded inside a if-endif guard. The condition of the if statement is the combination of the CONFIG_MCUX_COMPONENT_ prefix and the component name, which indicates everything insides the if-endif section belongs to a software component.
Please note that nested if-endif is not supported, and the if condition shall only contain one component name, combined condition with || or && is not supported either.
Here is the driver.uart CMakeLists.txt:
if (CONFIG_MCUX_COMPONENT_driver.uart) # component name is driver.uart
# component version
mcux_component_version(2.5.1)
# component data
mcux_add_source(
SOURCES fsl_uart.h
fsl_uart.c
)
mcux_add_include(
INCLUDES .
)
endif()
If a component definition is split into several cmake files, please use the same if(CONFIG_MCUX_COMPONENT_<component name>)-endif guard in all files data.
Kconfig
In Kconfig, the symbol for a component shall also start with MCUX_COMPONENT_ to be identical with cmake component name. Component configuration and dependency shall be recorded in Kconfig following the below pattern:
config MCUX_HAS_COMPONENT_driver.uart
bool
default y if MCUX_HW_IP_DriverType_UART # such MCUX_HW_IP_DriverType_UART is defined in device Kconfig.chip
config MCUX_COMPONENT_driver.uart
bool "Use driver uart"
select MCUX_COMPONENT_driver.common
depends on MCUX_HAS_COMPONENT_driver.uart # component dependency
# Configuration for driver.uart shall be put into the if-endif so that only driver.uart is selected, the configuration will be showed
if MCUX_COMPONENT_driver.uart
# Configuration for driver.uart
endif
About the dependency, please refer Complex Dependency chapter for details.
For multiple components belonging to one middleware set, please use menu to gather them together, like
menu "freertos-kernel(FreeRTOSConfig.h)"
config MCUX_COMPONENT_middleware.freertos-kernel
bool "middleware.freertos-kernel"
select MCUX_COMPONENT_middleware.freertos-kernel.extension
......
config MCUX_COMPONENT_middleware.freertos-kernel.cm33_non_trustzone
bool "cm33 non trustzone port"
default n
depends on (MCUX_HW_CORE_CM33 || MCUX_HW_CORE_CM33F)
config MCUX_COMPONENT_middleware.freertos-kernel.cm33_trustzone.non_secure
bool "cm33 trustzone, non secure port"
default n
depends on (MCUX_HW_CORE_CM33 || MCUX_HW_CORE_CM33F)
config MCUX_COMPONENT_middleware.freertos-kernel.tfm_ns
bool "TF-M NS support"
select MCUX_COMPONENT_middleware.freertos-kernel.cm33_non_trustzone
select MCUX_COMPONENT_middleware.tfm.ns
default n
help
OS wrapper for running inside TF-M non secure world
config MCUX_COMPONENT_middleware.freertos-kernel.extension
default n
bool "Task Aware Debugger (TAD) support"
......
endmenu
Component macro configurations will be generated in header files. Please refer to Config Headers chapter for details.
Supported Components
There are following components which are already enabled in MCUXpresso SDK: drivers, components/utilities, middlewares and RTOS. They are located under mcuxsdk/drivers, mcuxsdk/components, mcuxsdk/middlewares and mcuxsdk/rtos.
Base device and board specific drivers and components are located in the target device and board folder.
All software components are involved into build tree through the root mcuxsdk/CMakeLists.txt and mcuxsdk/Kconfig.mcuxpresso. You can check them with Kconfig GUI and select needed components into your example.
Component Naming
As you can see, in our build system, all components naming is in format MCUX_COMPONENT_<name> . The MCUX_COMPONENT_ prefix indicates that the data section is a software component. About the specific component name, currently they are generally following the format <major type>.<minor types>.<name>. The dot is used to separate component type and name. The minor type(s) is optional and can be more than one like driver.uart , middleware.fatfs and middleware.fatfs.mmc.
Most frequently used major types are:
Major Types |
Explanation |
Examples |
|---|---|---|
driver |
Base SDK drivers |
driver.uart, driver.clock |
component |
SDK components |
component.serial_manager, component.serial_manager_spi |
utilities |
SDK utility |
utilities.gcov, utilities.unity |
middleware |
Middlewares and RTOSes |
middleware.fatfs, middleware.freertos-kernel |
The above naming convention applies to both cmakes and Kconfigs. For Kconfig, normally all Kconfig symbols will be generated into header files as macros, so there will be macros like CONFIG_MCUX_COMPONENT_component.serial_manager=1 in the generated header file which will cause build failure because C language identifiers cannot contain punctuation mark dot. To resolve this, our build system intentionally remove such component naming symbols from generated header file. Please check MCUXpresso SDK Customized Kconfig Rules for more rules and details.