FRDM-MCXE247
Overview
The FRDM-MCXE247 board is a design and evaluation platform based on the NXP MCXE247 microcontroller (MCU). NXP MCXE247 MCU based on an Arm Cortex- M4F core, running at speeds of up to 112 MHz with a 2.70–5.5 V supply. The FRDM-MCXE247 board consists of one MCXE247 device with a 64 Mbit external serial flash (provided by Winbond). The board also features FXLS8974CFR3 I2C accelerometer sensor, one NMH1000 I2C Magnetic switch, three TJA1057GTK/3Z CAN PHY, Ethernet PHY, RGB LED, push buttons, and MCU-Link debug probe circuit. The board is compatible with the Arduino shield modules, Pmod boards, and mikroBUS. For debugging the MCXE247 MCU, the FRDM-MCXE247 board uses an onboard (OB) debug probe, MCU-Link OB, which is based on another NXP MCU: LPC55S16.
MCU device and part on board is shown below:
Device: MCXE247
PartNumber: MCXE247VLQ
Getting Started
Getting Started with MCUXpresso SDK for FRDM-MCXE247
Release Notes
This is an Early Access Release (EAR) for FRDM-MCXE247 developement board. It shall be used for pre-production development only.
Only drivers which has its example(s) in mcuxsdk/examples/_boards/frdmmcxe247/driver_examples folder were tested.
Supported Development Tools
MCUXpresso for VS Code v25.03
GCC Arm Embedded Toolchain
MCUXpresso SDK Release Notes for FRDM-MCXE247