# Training Zephyr Getting Started MCXN947 ## Recommended Zephyr Revision Importing the Zephyr repository during the Installation steps, we recommend starting with the latest Zephyr release. The Repository Importer tool will default to the latest Zephyr release. For more details, see [Zephyr Revision](./Zephyr-Lab-Installation-and-Preparation#Zephyr-Revision). ## Hardware Requirements These labs are written for the evaluation board listed below. However, these labs use sample applications in the Zephyr repository, and will easily run on other NXP boards supported in the Zephyr tree: * [FRDM-MCXN947](https://www.nxp.com/design/design-center/development-boards-and-designs/general-purpose-mcus/frdm-development-board-for-mcx-n94-n54-mcus:FRDM-MCXN947) * USB Type-C cable * This board integrates an on-board debugger, and the labs are written to use this debugger with the default MCU-Link CMSIS-DAP debug probe. ![FRDM-MCXN947](./pictures/Training-FRDM-MCXN947.png) ## Zephyr Lab Guides with VS Code This set of lab guides provide detailed steps to get started with Zephyr and the MCUXpresso extension for VS Code using the FRDM-MCXN947 board: * Lab 0: [Zephyr Lab Installation and Preparation](./Zephyr-Lab-Installation-and-Preparation) * Lab 1: [Zephyr Lab MCXN947 Hello World](./Zephyr-Lab-MCXN947-Hello-World) * Lab 2: [Zephyr Lab MCXN947 Kconfig](./Zephyr-Lab-MCXN947-Kconfig) * Lab 3: [Zephyr Lab MCXN947 Debug](./Zephyr-Lab-MCXN947-Debug) * Lab 4: [Zephyr Lab MCXN947 Devicetree](./Zephyr-Lab-MCXN947-Devicetree) * Lab Appendix: [Zephyr Lab Revert Workspace](./Zephyr-Lab-Revert-Workspace) ## Lab Notes - The lab steps are written for Windows 11. But Zephyr and NXP's tools, including the [MCUXpresso extension for VS Code](https://github.com/nxp-mcuxpresso/vscode-for-mcux/wiki), are also supported on Ubuntu and macOS. All the labs will work on each supported OS with minimal changes needed. - File Paths - The file paths used in these steps follow the Windows guidelines in the [Zephyr Getting Started](https://docs.zephyrproject.org/latest/develop/getting_started/index.html) documentation, to place the *zephyrproject* folder in the user path `c:\Users\\zephyrproject`. These steps reference the user name **NXP**, so the path provided in the steps is `c:\Users\NXP\zephyrproject`. Be sure to change this path to match your installation.