# Installer Update The installer is able to self-update whenever a new version is available. The update status can be checked in the toolbar of the application, in the top right corner. >**Note:** This update is different from components update. Components updates will be silently installed until a new version of the Installer is available. In order to continue to get components update, it is necessary to update the Installer to the latest version, using this feature. Once updated, components updates will resume. ![Update button](./pictures/nxp-installer-update-button.png) The icon will change depending on the update status of the application. The following states are possible: ## Up to date ![Up to date](./pictures/nxp-installer-up-to-date-button.png) The icon will be in its default state, without any indicators, and the tooltip will show the message **"Up to date"**. The user can click on the icon to open a different menu, where it is possible to refresh the application and check for updates. ![Update menu](./pictures/nxp-installer-up-to-date.png) ## Updates available ![Updates available](./pictures/nxp-installer-updates-available.png) The icon will show a pulsing green indicator and the tooltip will show the message **"An updated version of the app is available to install"**. The user can click on the icon to enter the update menu. ![Update menu](./pictures/nxp-installer-updates-available-menu.png) Clicking on the update button will fetch the newest available version of the Installer application in the background and install once the application is closed. ## Updating ![Updating](./pictures/nxp-installer-updating-button.png) The icon will show a pulsing blue indicator and the tooltip will show the message **"Updates are installed and will be applied after application restart"**. Opening the update menu will display the same message. ![Update menu](./pictures/nxp-installer-updating-menu.png) ## Update server unavailable ![Update server unavailable](./pictures/nxp-installer-update-server-offline-button.png) The icon will show a pulsing red indicator and the tooltip will show the message **"Could not connect to update server. Updates are unavailable"**. Usually this is due to being disconnected from the Internet, but may also occur on improperly configured networks. Entering the update menu will show a similar message. ![Update menu](./pictures/nxp-installer-update-server-offline-menu.png) In the case that the connection to the Internet is restored, it is necessary to restart the Installer application to restore network connectivity. ## Loading The icon will show a pulsing red indicator and the tooltip will show the message **"Loading"**. Entering the update menu will show a loading message. Once the application has connected to the update server, the message will update. This usually takes less than a few seconds, but it might take more on slower networks. ![Loading](./pictures/nxp-installer-loading.png) ## Post-install After the updates are downloaded, the user will be notified via a console message. ![Updates finished](./pictures/nxp-installer-updates-finished.png) After closing the application, the updates will be applied automatically.