# Getting Started with MCX using Application Code Hub ## Objectives NXP customers can design the MCX microcontroller family into many different applications. NXP provides the Application Code Hub to help customers access example solutions created by NXP Engineers. The examples solve common requirements in applications using the NXP MCUXpresso SDK components. The examples expand on the base examples included in the SDK. The following lab guides walk through the steps to evaluate 2 different projects from the Application Code Hub (ACH). The labs require FRDM hardware and application specific Shield boards. Links are provided to help aquire all of the required hardware and software. ## Lab Procedures Each guide can be completed independently. There is no required order. User's can follow the Installation and Preparation guide to correctly set up their system. - [Installation and Preparation](./MCX-Lab-Installation-and-Preparation.md) - [FRDM-MCXN947 Facial Recognition](./MCX-Lab-Facial-Recognition.md) - [FRDM-MCXA153 FreeMASTER Heart Rate](./MCX-Lab-Heart-rate-demo.md) ```{toctree} :maxdepth: 1 MCX-Lab-Installation-and-Preparation MCX-Lab-Facial-Recognition MCX-Lab-Heart-rate-demo ```