# Working with MCUXpresso SDK NXP provides a large series of open source drivers, middleware, and reference example applications to speed your software development. These come in different flavors: - *[GitHub](https://github.com/NXPmicro/mcux-sdk)* repository - Zip package SDK built upon preferred HW target, host OS, toolchain at *[MCUXpresso SDK](https://mcuxpresso.nxp.com/en/welcome)* MCUXpresso for VS Code offers the possibility to install and use these sources with this extension. ## Import remote Git repository A special tab option on the **Imported Repository** view will allow the user to specify the details about the remote repository. ![Install remote SDK](./pictures/nxp-import-sdk-remote.png) Once this process is finished, **Imported Repositories** view will display all downloaded SDKs from that repository. ![Imported remote SDK](./pictures/nxp-view-imported-sdk.png) By default, "main" revision is set. If other revision is needed, check the expanded list. ![Install revision SDK](./pictures/nxp-sdk-revisions.png) By default, "west.yml" manifest file is used to import, if other manifest file is needed check the "Use custom manifest file" checkbox and select an option. ![Install manifest SDK](./pictures/nxp-sdk-manifest.png) ## Import standalone MCUXpresso SDK zip archive Another possibility is to install an MCUXpresso SDK from a zip archive (Downloaded from *[MCUXpresso.NXP.com](https://mcuxpresso.nxp.com/en/welcome)*). ![Install archive SDK](./pictures/nxp-import-sdk-archive.png) The extension will check for compatibility issues, then extract the archive at the specified location. If the user chooses to use the "Create Git repository" option a git repository will be initialized at the SDK location, with the branch name `SDK_.`. Afterwards, a git commit will be performed with all of the files present in the SDK. Archive SDKs also have an update branch which will be created after these steps. The branch is tagged from the main SDK branch. Having a Git repository that contains the SDK source code allows the users to keep track of the changes they made in the SDK source code and to switch between SDK versions, however the option of handling the git repository on their own is also available. ## Import MCUXpresso SDK using SDK Builder It is also possible to import an MCUXpresso SDK archive directly from the extension, using the SDK Builder. ![SDK Builder](./pictures/nxp-import-sdk-builder.png) After selecting a package (which can be either a board or a device) and a version, information regarding the SDK package will be displayed. ![SDK Builder Package Information](./pictures/nxp-import-sdk-package-info.png) The view will display the related boards and devices of the selected package, along with a description and an image, if available. Additional information can be obtained by visiting the *"View on NXP.com"* hyperlink, present under the package description. Similar to a local MCUXpresso SDK archive, the option to create a Git repository is also available. The license of the package can be inspected by clicking on the *license* hyperlink. A new window with a preview will be opened on the side. ![SDK Builder License Preview](./pictures/nxp-import-sdk-license.png) After agreeing to the license, the selected package will be downloaded and will undergo the same import process as the local archive. ## Create, build and debug the project For creating, building and debugging the project, the standard steps described in {doc}`Create Project ` document, {ref}`Build Project ` section and {doc}`Debug ` document should be followed. >**Note:** For MCUXpresso SDK 2.x version, the examples are only imported as "Freestanding" projects. That means, the project files are copied in the newly created project folder, while the SDK needed files are kept as links in the reference MCUXpresso SDK folder. Being the single "App type" option, this is the default so the "App type" field is not displayed in the wizard form as it is for other repository choices. In comparison, for MCUXpresso SDK 24.12 version or newer, "Repository" and "Freestanding" options are available, so the user can choose between keeping the project example in the repository, or copying the project sources in an outside directory (freestanding). ## Build Configuration ### SDK version 24.12 or newer (changing-configuration-file)= ### Changing configuration file Project configuration is managed through Kconfig configuration files (`.conf` files). These files allow you to customize component selection, feature enablement, and various build settings. To change the configuration file go to `Build Configuration` from the **Projects** view and edit the build configuration that is currently used. From the `Config file` drop-down menu select one or multiple files and make your desired changes. Press `Save` to apply the changes. ![Conf files](./pictures/nxp-sdk-conf-files.png) The list of available configuration files is automatically detected by searching for `.conf` files in the project directory and `CMakePresets.json` file. If your desired configuration file is not listed, you can manually add the path using the "+ Add configuration file path" entry in the drop-down menu. ![Add conf files](./pictures/nxp-sdk-add-conf-file.png) For detailed information about the configuration system and configuration priority, please refer to the [MCUXpresso SDK Configuration System documentation](https://mcuxpresso.nxp.com/mcuxsdk/latest/html/develop/build_system/Configuration_System.html). ### SDK version 2.16 or older #### Changing floating point type Project configuration options offers possibility to change the floating point ABI for MCUXpresso SDK based projects. If needed to do so, go to the build configuration used by the project, select Edit -> Go to the Floating Point option and select from the available list displayed. Press the `Save` button to apply the changes. ![Floating point](./pictures/nxp-floating-point.png) This change will be saved in the `CMakePresets.json` file as FPU_TYPE and FPU_ABI cacheVariables. Simply remove these settings in order to revert to the default project options (if needed to identify this, search for set_floating_point function in `./__repo__/tools/cmake_toolchain_files/mcux_config.cmake` file). #### Changing library type Configuration options provide option to switch C/C++ library type. Select Configure -> Set Library Type from project context menu. This will allow selecting from the available library types. Newlib and Newlib-nano are available by default as they are embedded into the Arm GNU Toolchain distribution. Redlib is NXP variant of (non-GNU) ISO C90 standard C library, with some C99 extensions. If you need a smaller application size and don't need the additional functionality of the C99 or C++ libraries, we recommend the use of Redlib, which can often produce much smaller applications. ![Library type](./pictures/nxp-library-type.png) This change will be saved in the CMakePresets.json file as LIBRARY_TYPE cacheVariables. If needed to identify details on how the library type option is used, follow set_library function in `./__repo__/tools/cmake_toolchain_files/mcux_config.cmake` file. ## Redlib extensions to C90 >**Note:** Redlib is provided by the NXP Toolchain Add-on pack distributed by the MCUXpresso Installer and it comes installed on top of an Arm GNU Toolchain distribution. Be sure you have 12.3.2 or newer version of NXP Toolchain Add-on in order to have Redlib support added. Alternatively, the toolchain provided by MCUXpresso IDE (in case there is already an existing installation on the machine) can be used, which already contains Redlib support. Also, MCUXpresso SDK 2.15 or newer has to be used in order to provide integration support of Redlib. Although Redlib is basically a C90 standard C library, it does implement a number of extensions, including some from the C99 specification. These include: - Single precision math functions - Single precision implementations of some of the math.h functions such as sinf() and cosf() are provided. - stdbool.h - An implementation of the C99 stdbool.h header is provided. - inttypes.h - An implementation of the C99 inttypes.h header is provided. - itoa - itoa() is a non-standard library function which is provided in many other toolchains to convert an integer to a string. To ease porting, an implementation of this function is provided, accessible via stdlib.h. More details can be found later in this chapter. ## Library variants Each C library family is provided in a number of different variants: None, Nohost and Semihost. These variants each provide a different set of 'stubs' that form the very bottom of the C library and include certain low-level functions used by other functions in the library. Each variant has a differing set of these stubs, and hence provides differing levels of functionality: - Semihost(-mb) - This library variant provides an implementation of all functions, including file I/O. The file I/O is directed through the debugger and is performed on the host system (semihosting). For example, printf/scanf uses the debugger console window and fread/fwrite operates on files on the host system. Note: emulated I/O is relatively slow and can only be used when debugging. Note that mb library variants may optionally be selected for enhanced semihost performance with the penalty of slightly larger RAM usage. - Semihost(-mb)-nf (no files) - Redlib only. Similar to Semihost, but only provides support for the 3 standard built-in streams: stdin, stdout, stderr. This reduces the memory overhead required for the data structures used by streams, but means that the user application cannot open and use files, though generally this is not a problem for embedded applications. - Nohost and Nohost-nf - This library variant provides the string and memory handling functions and some file-based I/O functions. However, it assumes that you have no debugging host system, thus any file I/O does nothing. However, it is possible for the user to provide their own implementations of some of these I/O functions, for example, to redirect output to the UART. - None - This has literally no stub and has the smallest memory footprint. It excludes low-level functions for all file-based I/O and some string and memory handling functions. In many embedded microcontroller applications it is possible to use the None variant by careful use of the C library, for instance avoiding calls to printf(). If you are using the wrong library variant, then you will see build errors in the form: ``` Linker error "Undefined reference to ‘xxx’ " ``` For example for a project linking against Redlib(None) but using printf() : ``` … libcr_c.a(fpprintf.o): In function `printf': fpprintf.c:(.text.printf+0x38): undefined reference to `__sys_write' fpprintf.c:(.text.printf+0x4c): undefined reference to `__Ciob' ``` Or if linking against NewlibNano(None): ``` … libc_nano.a(lib_a-writer.o): In function `_write_r': writer.c:(.text._write_r+0x10): undefined reference to `_write' ``` In such cases, simply change the library hosting being used (as described below), or remove the call to the triggering C library function. ## Changing toolchain for an existing project When importing a project or an example from the repository you are required to choose a toolchain to be associated to the project. The associated toolchain can be modified later for an existing project. To change it, right-click on the project, navigate to "Configure", and select "Associate Toolchain". For more details, please refer to the {ref}`Toolchain Management ` documentation. ![Associate toolchain](./pictures/nxp-associate-toolchain.png) ## Changing the associated repository for an existing project You can also change the repository associated to an existing project. To do this go to the context menu of the project, select "Configure" and then "Associate Repository", you should now see all the available MCUXpresso SDK repositories and select the desired value. The already associated repository is marked. ![Associate repository](./pictures/nxp-associate-repository.png) ## Changing the associated device/package for an existing project MCUs are commonly available in a range of package types. Different packages may impact the options available on the MCU external pins, for example, the number of GPIO lines. MCUXpresso for VS Code makes no use of this package type however it is significant to MCUXpresso Config Tools. From the **Projects** view, for "MCU" virtual node, select "Change Device/Package". ![Change package](./pictures/nxp-change-package.png) The quick pick displays a list of supported devices and packages available for the current project. These devices are derivatives of the currently selected MCU. Selecting a new device or package automatically updates the project configuration. ![Select package](./pictures/nxp-select-package.png) ## Project Integrated Terminal Open MCUXpresso Terminal specific for the project using project menu -> Open in Integrated Terminal. The opened MCUXpresso terminal will have the environment completely configured for the project and the associated repository type, including system specific variables, virtual python environment (if available), utility tools access (i.e. west, available debug probe software). Example command to build the project appears in green. The command is constructed specific for the project and it can be used as is for a quick west build. ![Build in terminal](./pictures/nxp-terminal-mcuxsdk-build-project.png)