# MCX Lab Facial Recognition ## Objectives In this lab, you will learn: - How to import an example in the VS Code workspace using Application Code Hub - How to build, clean, debug, and run the example - How to connect the Serial Monitor for UART console - How to navigate and edit files in the Explorer view - How to modify project/code related to the Neural Processing Unit (NPU) ## Facial Recognition Lab After successfully installing the VS Code extension for MCUXpresso, let’s go through the detailed steps to use NXP's Application Code Hub to run the Facial Recognition Lab on MCX FRDM board. ### 1. Verify Installation The prework instructions should be completed before starting this lab. The instructions walk through the installation for the required software. After finishing, the system should have the following: Visual Studio Code - Base software tool distributed by Microsoft MCUXpresso for Visual Studio Code Extension - NXP developed extension to configure VS Code for embedded MCU development MCXUXpresso Installer - required to install 3rd party tools for MCUXpresso projects to correctly import/build/debug. FRDM-MCXN947 SDK 2.14.0 - required to provide software libraries for middleware and drivers referenced in the example ### 2. Import Project with Application Code Hub The Application Code Hub (ACH) repository enables engineers to easily find microcontroller software examples, code snippets, application software packs and demos developed by our in-house experts. This space provides a quick, easy and consistent way to find microcontroller applications. Find more information at [www.nxp.com/ach](https://www.nxp.com/ach) The MCUXpresso for VS Code extension has integrated the Application Code Hub into the development environment. The extension provides an Import Wizard to simplify adding examples from the Application Code Hub. The wizard handles the steps required to clone the selected project repository. >**Note:** The Application Code Hub examples are delivered from GitHub at [www.github.com/nxp-appcodehub](https://www.github.com/nxp-appcodehub) The integrated viewer makes it easier for customers to explore. Alternatively, customers can manually add the projects using traditional methods to clone GitHub repositories and importing the local project folder. Here are the steps to import a new Example from the Application Code Hub: 1. Go to the Quick Start Panel 2. Select Application Code Hub ![Build project](./pictures/mcx-gs-facedetect-1.png) 3. Filter visible examples (MCX + ML/AI) - Go to the filter section next to the Search bar and select two filters. **MCX** in the Device Families Section and **ML/AI** in the Categories section of the filters. ![Build project](./pictures/mcx-gs-facedetect-2.png) ![Build project](./pictures/mcx-gs-facedetect-3.png) 4. Search for Keywords in Examples Search for the keyword **'face detect'**. Select the demo ***"multiple person detection mcxn947"***. ![Build project](./pictures/mcx-gs-facedetect-5.png) 5. Read Overview of Facial Recognition Demo The Application Code Hub provides a consistent Readme Overview for every project. The Facial Recognition demo overview is previewed after clicking on the application card. Scroll through the readme to become familiar with the available contents like required **hardware**, **software** and **setup** instructions. ![Build project](./pictures/mcx-gs-facedetect-6.png) 6. Select Destination for Project The wizard automatically provides a prompt to browse to a desired destination folder. Choose the Folder C:\VS-Code-Projects\Facial-Recognition. ![Build project](./pictures/mcx-gs-facedetect-7.png) 7. Import Project into Workspace Select **Import Project(s)** after entering the desired location. If a valid project is not available, the wizard only displays **Import Repository**, to allow a code repo, without a project, to be added to workspace. 8. Select Detected Project(s) The import wizard will scan the example repo and list valid projects that were discovered. This allows the user to select only the projects they want created. Select the **mcuxpresso** project listed at the top of the VS Code window below the Workspace Search bar. 9. Choose a Toolchain The last selection is to identify the Compiler toolchain to be used for the project. GCC will be used for this project. Select **Arm GNU Toolchain 12.2.Rel1** (Or latest version available from MCUXpresso Installer prework) ![ACH Choose a Toolchain](./pictures/mcx-gs-heartrate-1-select-toolchain.png) At this time the wizard completes importing the project into the workspace. A ***Successful Conversion*** notification is displayed at the bottom of the screen. It is important to recognize that the selected Facial Detection example is a working project within the MCUXpresso IDE (Eclipse based). The VS Code extension has a ability to convert an existing project with a few requirements. ![ACH Succesful Convert](./pictures/mcx-gs-heartrate-1-successful-convert.png) ### 3. Navigating a Project in VS Code The MCUXpresso for VS Code extension includes a **Projects** section to help users access useful project information. A user can review and modify project information with the following steps. 10. Review Project Details Project details are shown in the Dropdown menu of the Projects Section in the MCUXpresso Extension Navigation Pane - ***Repository Information***: Verify the necesary SDK is associated with converted project. >**Note:** Step 2 below details how this can be corrected. - ***MCU***: Understand the targeted device and board. - ***Memory***: View quick memory map of project. - ***Build Configurations***: Select build configuration from available list (i.e. Debug or Release). ![Build project](./pictures/mcx-gs-heartrate-1-project-details.png) 11. Associate the Required MCUXpresso SDK Sometimes, Projects imported/converted from the Application Code Hub do not automatically have a valid SDK associated to them. This can be caused by the required SDK not being installed and imported into the workspace. The prework for this lab installed the expected FRDM-MCXN947 SDK. The import wizard should associate the information from the project with the available SDK. If Project information is blank (i.e. Repository Information), you must manually associate an SDK with a project. The Following steps will assign the FRDM-MCXN947 SDK to the project: - **Right Click** on the Project to fix. - In the Drop-down menu, **Select Configure -> Associate Repository** - **Select SDK-FRDM-MCXN947** from a list of availble SDK repos listed at the top of VS Code window below search bar. ![Build project](./pictures/mcx-gs-heartrate-1-associate-sdk.png) Now the correct information should be displayed for the project. >**Note:** If a valid SDK is not assigned, a project will fail to build with an Error message noting that a CMAKE build configuration is not located. 12. Working with Source Files Go to Explorer -> Click on MCX N Face Recognition and you will find the Source files like main.cpp etc in the Dropdown ![Build project](./pictures/mcx-gs-heartrate-1-source-files.png) ### 4. Build the application The *MCX Lab Facial Recognition* project needs to build the application image. After the code builds without any errors, the application can be run on the FRDM board. If not done already, connect the USB-C cable to J17 to power the FRDM board. This provides power to the board and the onboard debugger provides a USB-UART bridge to interface with the Serial monitor. 13. Build the project by clicking the **Build Selected** icon. ![Build project](./pictures/mcx-gs-facedetect-11.png) After the build, the debug console window displays the memory usage (or compiler errors if any). ![Build output](./pictures/mcx-gs-facedetect-build-2.png) ### 5. Debug the application This section uses the GDB debugger to connect to the MCU, and program the flash. 14. Click the play icon to **Debug** the application: ![Debug project](./pictures/mcx-gs-facedetect-build-6.png) 15. The execution will pause. To continue execution click **Continue** on the debug options. ![Continue debugging](./pictures/training-zephyr-continue-debugger.png)
16. After building the application, Right click on the Project Name i.e., 'MCX-N-Facial Recognition' and select 'Flash the Selected Target'. ![Flash the Selected Target](./pictures/mcx-gs-facedetect-build-8.png)
17. After the .elf file is flashed to the target device, the camera starts detecting the face and displays the image on the LCD display ![The camera starts detecting the face and displays the image on the LCD display](./pictures/mcx-gs-facedetect-build-7.png)
18. Record the NPU Inference Time/Latency for comparison ### 6. Modify NPU In the Explorer tab, go to the imported project i.e., MCX-N-Face-Recognition and click on the file model_data.s ![Find the file to modify the NPU model](./pictures/mcx-gs-facedetect-modify-npu-1.png) In line 43, change **face_detect_converted.tflite** to **face_detect.tflite** and rebuild the model i.e., repeat Steps 4 and 6 to build and flash the application. ![Change the line to face_detect.tflite](./pictures/mcx-gs-facedetect-modify-npu-2.png) You will now see that the performance of the model without using the NPU is now 30 times slower and the latency is higher. > The Facial Recognition Lab is now completed. Return to [Getting Started with MCX using Application Code Hub](./Getting-Started-with-MCX-using-Application-Code-Hub.md)