# Zephyr lab installation and preparation
In this lab, you will learn to install/import the tools below. This guide is written for Windows11. Linux or macOS can also follow similar steps.
The necessary installations include:
- Visual Studio Code
- MCUXpresso Extension for VS Code
- Dependencies for Zephyr development, including the Zephyr SDK
- Zephyr Repository in VS Code
- (Optional) MCUXpresso SDK Repository in VS Code
## Software Versions
This lab guide was written with the following versions
- MCUXpresso extension for VS Code v25.3.72
- MCUXpresso Installer v24.12
- Zephyr v4.1.0
- Zephyr SDK v0.17.0
- LinkServer v25.3.31
## Zephyr Revision
Before importing the Zephyr repository, determine the Zephyr revision to checkout. Upstream Zephyr manages the revisions with Git: Zephyr releases have Git tags for the versions, or the latest code is in the `main` branch.
For development, it is ideal to use a Zephyr release. Releases go through the Zephyr Project's release flow and quality checks. This is why the Repository Importer in the MCUXpresso extension defaults to the latest Zephyr release. To learn more about Zephyr releases, see [Releases](https://docs.zephyrproject.org/latest/releases/index.html).
One resource available to confirm support in different revisions is the Zephyr Project documentation. For example, the [Supported Boards and Shields](https://docs.zephyrproject.org/latest/boards/index.html) is a living document for the hardware currently in the `main` branch, and is updated frequently.
## Installation Steps
### VS Code and MCUXpresso extension
1. To install Visual Studio Code (VS Code), download the installer here: https://code.visualstudio.com/download
2. Open VS Code, and install the MCUXpresso extension.
a. Click the extensions view **( CTRL+Shift+X )**
b. In the search field at the top of the extension view type **MCUXpresso**
c. Click the **Install** button

The MCUXpresso extension will be added to the installed list after successful installation.
### Zephyr dependencies and debugger tools
Zephyr development environment needs some host dependencies like: CMake, Python, Devicetree, Zephyr SDK, and other… LinkServer is also required to debug with the NXP on-board probes.
> **Note** this lab guide assumes a LinkServer debug probe is used, which is default on the evaluation boards. When utilizing other supported debug probes, this installer can additionally integrate support for Segger JLink and PEmicro tools.
3. Open the MCUXpresso Extension. In the Quickstart Panel, click **Open MCUXpresso Installer**

4. After selecting the install options: **Zephyr Developer**, and **LinkServer** click the **Install** button. The status bar at the bottom shows how the installation is progressing.

5. Restart VS Code to enable the changes to environment variables.
## Import the software repositories
6. To import the Zephyr repository, open the MCUXpresso view in VS Code and click **Import Repository** in the Quickstart Panel.

7. Select **Zephyr** Repository, choose the latest revision **v4.1.0**, finally choose the folder location **C:\Users\...\zephyrproject**. When finished, click **Import**.

> **Note** This import step takes a long time to clone the Zephyr repo, and dependency repos (currently 70!). VS Code shows a progress bar pop-up with the status of the West tool as it clones all the repos. The repository should be added to the Imported Repository view once the import is successful.
8. Optionally, the MCUXpresso SDK repository can be imported the same way. This is not required when working with Zephyr. But the debugger guide in [Training Zephyr Getting Started](./Training-Zephyr-Getting-Started.md) shows how to add the Peripheral Register view to the debugger, and this requires some SVD files located in the MCUXpresso SDK repository.
Select the following board settings to import the MCUXpresso SDK repository:
- `Repository` select **MCUXpresso SDK - 24.12 or newer**
- `Revision` choose the latest release **v25.03.00**
- `Location` select the folder location: **C:\Users\\...\mcux-sdk**
- Click **Import**

The repositories are successfully added to the Imported Repository view once the import is successful.

9. To import any example application from the Zephyr Repository, click **Import Example from Repository** in the Quickstart Panel.

10. To ensure successful installation, follow the steps in the Hello World guide to run the hello_world example from the Zephyr repo.
> Lab completed. Return to the Zephyr Labs Overview [Training Zephyr Getting Started](./Training-Zephyr-Getting-Started.md)